cancel
Showing results for 
Search instead for 
Did you mean: 

DMA 0 transfer is working

ComAp R&D
Associate
Posted on June 20, 2018 at 14:12

Hello,

because of my mistake I call function:

HAL_StatusTypeDef HAL_DMA_Start_IT(DMA_HandleTypeDef *hdma, uint32_t SrcAddress, uint32_t DstAddress, uint32_t DataLength)

with params:

HAL_DMA_Start_IT(hmmc_xy, from_addr, to_addr, 65536);

The function write 0 to SxNDTR, because the register is 16bit wide. In spite of that transfer of 65536 is always performed.

How it is possible?

Setting on MCU STM32F777II,

{

.Instance = DMA2_Stream3,

.Init.Channel = DMA_CHANNEL_4,

.Init.Direction = DMA_PERIPH_TO_MEMORY,

.Init.PeriphInc = DMA_PINC_DISABLE,

.Init.MemInc = DMA_MINC_ENABLE,

.Init.PeriphDataAlignment = DMA_PDATAALIGN_WORD,

.Init.MemDataAlignment = DMA_MDATAALIGN_BYTE,

.Init.Mode = DMA_PFCTRL,

.Init.Priority = DMA_PRIORITY_VERY_HIGH,

.Init.FIFOMode = DMA_FIFOMODE_ENABLE,

.Init.FIFOThreshold = DMA_FIFO_THRESHOLD_1QUARTERFULL,

.Init.MemBurst = DMA_MBURST_INC4,

.Init.PeriphBurst = DMA_PBURST_INC4,

}

#ndtr #dma #0-len
This discussion is locked. Please start a new topic to ask your question.
0 REPLIES 0