2009-08-26 12:30 AM
DIY a emluator for STM32
2011-05-17 4:21 AM
Hi all,
There is a kind of smart and open emluator for cortex-m3 -- CooCox Colink,which supports all Arm Cortex-M3 devices. you can just do it yourself using the open circuit schematic diagram. It connects the JTAG interface from target board (ARM processors) to PC USB port, supports source level debugging and Flash programming. You can debugs the ARM Cortex-M3 processors through Realview MDK or EWARM. For more infomation,You can visit . [ This message was edited by: ahnniu on 26-08-2009 13:06 ]