2019-11-07 1:56 AM
Hello everybody,
I use the DISCO L475VG_IOT1A board with the onboard Wi-Fi module Inventek ISM43362-M3G-L44.
I would like to start an access point with an HTTP server.
I use this MBED example: os.mbed.com/teams/ST/code/DISCO_L475VG_IOT01-wifi_http_server/
The board acts as a Wifi client in this example.
If I now start the AP Direct Connect mode instead of the Wifi Client mode, the HTTP server will not work properly anymore.
At the first website visit I receive the http GET command.
After that, I receive an error message regardless of the website visit:
ES-WIFI Initialized.
Firmware: C3.5.2.5.STM
> es-wifi module connected
>Start HTTP Server...
>Socket: 0
> HTTP Server Started
> Wifi_ReceiveData - Socket: 0
resp: GET / HTTP/1.1
Accept: text/html,application/xhtml+xml,application/xml;q=0.9,*/*;q=0.8
Accept-Language: de-DE
Upgrade-Insecure-Requests: 1
User-Agent: Mozilla/5.0 (Windows NT 10.0; Win64; x64) AppleWebKit/537.36 (KHTML, like Gecko) Chrome/70.0.3538.102 Safari/537.36 Edge/18.18362
Accept-Encoding: gzip, deflate
Host: 192.168.10.1:8022
DNT: 1
Connection: Keep-Alive
OK
>
respLen: 377
Send Webpage
StopStart Server
> Wifi_ReceiveData - Socket: 0
resp: -1
ERROR: Unknown Error
Usage: R0
> ation/xhtml+xml,application/xml;q=0.9,*/*;q=0.8
Accept-Language: de-DE
Upgrade-Insecure-Requests: 1
User-Agent: Mozilla/5.0 (Windows NT 10.0; Win64; x64) AppleWebKit/537.36 (KHTML, like Gecko) Chrome/70.0.3538.102 Safari/537.36 Edge/18.18362
Accept-Encoding: gzip, deflate
Host: 192.168.10.1:8022
DNT: 1
Connection: Keep-Alive
OK
>
respLen: 32
According to inventeksys (www.inventeksys.com/iwin/getting-started-guide/), this error message reads: "And if by chance the eS-WiFi module was not connected to a server issuing an R0 command would generate the output:"
-1
ERROR: Unknown Error
Usage: R0
>
After receiving data, the server is stopped (P5 = 0) and started (P5 = 1) using the AT commands.
2020-09-06 1:38 AM
Hello my friend
Do you know how to use the wifi module (ISM43340-M4G-L44-10 CF) of the stm32h7b3i-dk board?
Any example of a WIFI http server with stm32h7b3i-dk ???
2020-10-03 11:47 PM
the same happens to me
manage to correct the problem ??
2020-12-03 3:12 AM
Hi, I've been having a related issue when the request for a download from S3 appears to be above approx 11,000 bytes. I commented out the command for the Timeout and I get a slightly more detailed error now as a result of issuing the R0 command:
[TCP SSL] Packet reception failed: 5003\r\nERROR: Unknown Error\r\nUsage: R0