Skip to main content
bagrowicz
Associate II
August 25, 2009
Question

difference

  • August 25, 2009
  • 2 replies
  • 772 views
Posted on August 25, 2009 at 18:12

difference

    This topic has been closed for replies.

    2 replies

    bagrowicz
    bagrowiczAuthor
    Associate II
    May 17, 2011
    Posted on May 17, 2011 at 13:21

    Hi!

    Is there any differene between STM32F103R6T6 (NRND) & STM32F103R6T6A??

    I know that ''A'' or blank1 is some internal code:

    ''For STM32F103x6 devices with a blank Internal code, please refer to the STM32F103x8/B datasheet available from the ST website: www.st.com.'';

    So if i buy STM32F103R6T6 i've got STM32F103R8???

    16-32micros
    Associate III
    May 17, 2011
    Posted on May 17, 2011 at 13:21

    Hi,

    If you buy a ''STM32F103R6T6'' , we {STMicroelectronics :-)} will send you ''STM32F103R6T6A'' device which is a Performance line - LQFP64 ad having 32Kbytes of Flash.

    STM32F103R6T6 without ''A'' at the end ; is no more existing now, However Two years ago it was the same device as ''STM32F103x8/B'' having the upper part of the Flash is not fully tested and qualified by our manufacturing.

    This note in our data-sheet is for our existing customers who already have in their production the old STM32F103R6T6.

    Hope this helps you.

    Cheers,

    STOne-32.

    [ This message was edited by: STOne-32 on 25-08-2009 21:43 ]