cancel
Showing results for 
Search instead for 
Did you mean: 

difference

bagrowicz
Associate II
Posted on August 25, 2009 at 18:12

difference

2 REPLIES 2
bagrowicz
Associate II
Posted on May 17, 2011 at 13:21

Hi!

Is there any differene between STM32F103R6T6 (NRND) & STM32F103R6T6A??

I know that ''A'' or blank1 is some internal code:

''For STM32F103x6 devices with a blank Internal code, please refer to the STM32F103x8/B datasheet available from the ST website: www.st.com.'';

So if i buy STM32F103R6T6 i've got STM32F103R8???

16-32micros
Associate III
Posted on May 17, 2011 at 13:21

Hi,

If you buy a ''STM32F103R6T6'' , we {STMicroelectronics :-)} will send you ''STM32F103R6T6A'' device which is a Performance line - LQFP64 ad having 32Kbytes of Flash.

STM32F103R6T6 without ''A'' at the end ; is no more existing now, However Two years ago it was the same device as ''STM32F103x8/B'' having the upper part of the Flash is not fully tested and qualified by our manufacturing.

This note in our data-sheet is for our existing customers who already have in their production the old STM32F103R6T6.

Hope this helps you.

Cheers,

STOne-32.

[ This message was edited by: STOne-32 on 25-08-2009 21:43 ]