cancel
Showing results for 
Search instead for 
Did you mean: 

Difference between ADC dual mode and 2 ADCs in independent mode

j3lda
Associate II
Posted on January 29, 2015 at 18:40

Hello, I am using STM32F3 Discovery kitand I need to measure 2 signals at the same time. It seems to me that there are to possibilities: 1) use regular simultaneous dual mode, 2) use 2 ADC's, both in regular single independent mode and triggered by the same timer.

What is the difference between these to possibilities? Or doesn't matter which way I choose for my application? 

Thank you for answeres.  
1 REPLY 1
Posted on January 29, 2015 at 18:46

When they are bonded you only need ONE DMA channel/operation. It's clean and simple, and while I'm sure other methods could perhaps be employed they would seem to be unnecessarily complicated.

Tips, Buy me a coffee, or three.. PayPal Venmo
Up vote any posts that you find helpful, it shows what's working..