cancel
Showing results for 
Search instead for 
Did you mean: 

DfuSe Demo crashes during Verify

rm2399
Associate III
Posted on October 15, 2013 at 12:06

Hi

I think it is not a problem of Win7.

I have the same problem here. I Generate a DFU file with the DFU file manager.

Programming with DfuSe Demo works without problems. But when comparing the program crashes.

When I download the program from the STM32F407 device, then does the comparison.

In DFU file manager I use the parameter read by DfuSe Demo.

VID: 0483

PID: DF11

Version: 2200   (Question: Where in the data sheets I find the correct PID and version number?)

Target ID: 00 Internal Flash
This discussion is locked. Please start a new topic to ask your question.
0 REPLIES 0