2018-05-29 08:45 PM
Hi ! I have designed a board with stm32f765 (LQFP100) but I got a problem with it when I test this board. I connect the board through usb cable with st link v2 and the ST Link Utility can detect this stm32f7 but when I download the code from Keil C to it, the stm32f7 got damaged because I find that vdd and vss pin are connected inside the chip. I try to find the reason and I think the reason is I don't configure for Boot0 pin. So I design another board with schematic image below. Can someone tell me that it is correct schematic ? I don't want to be failed again. Thank you.
2018-05-29 10:03 PM
Hello,
application note
gives you minimum requirements you have to take care of for proper hardware design.Best regards,
Tilen
2018-05-30 01:50 AM
,
,
Thank you ! I will check it again
2018-05-30 12:04 GMT+07:00 Tilen MAJERLE <,st-microelectronics@jiveon.com>,:
STMicroelectronics Community
<,https://community.st.com/?et=watches.email.thread>,
Re: Design for stm32f7 to programming
reply from Tilen MAJERLE
<,
in STM32 MCUs Forum - View the full discussion
<,https://community.st.com/0D70X000006SpYJSA0