2013-02-22 12:12 AM
Hi,
I am trying to make a simple delay function using a timer but i get weird results .Here is some of the code void TIMERS_init(){ TIM3->PSC = 23999; // f timer = fclk / 24000 => 1kHz TIM3->ARR = 0xFFFF; TIM3->CR1 = TIM_CR1_CEN; DBGMCU->CR = DBGMCU_CR_DBG_TIM3_STOP;}void Delay_ms(uint16_t ms){ TIM3->CNT = 0; while (TIM3->CNT < ms){}}while(1){
GPIOC->ODR ^= GPIO_ODR_ODR8; Delay_ms(500); //delay 0.5 sec GPIOC->ODR ^= GPIO_ODR_ODR8; Delay_ms(500); //delay 0.5 sec}The while in main is to test that the blue LED blinks at 2 Hz .I am using keil 4 . In debug if i run step by step works fine , but in continuously run the LED is half bright (probably is on and off at a high frequency) . I can't understand why because the prescalar remains set .2013-02-22 12:35 AM
On a VL-Discovery board? Or something else?
Did you enable the TIM3 clocks? What frequency do you see on a scope? Post sufficiently complete examples if you want support.2013-02-22 2:17 AM
STM32-discovery with 32F100 uc .
Yes , i enabled the timer clk . I don't have a scope . ________________ Attachments : Source_Code.rar : https://st--c.eu10.content.force.com/sfc/dist/version/download/?oid=00Db0000000YtG6&ids=0680X000006HznG&d=%2Fa%2F0X0000000bSo%2Fh4gOY5ZIGYHyrBe2m.y.Wpc3kVJPeaQah9GXtNCJMaw&asPdf=false2013-02-22 3:27 AM
void Delay_ms(uint16_t ms){
TIM3->ARR = ms; TIM3->CNT = 0; while((TIM3->SR & TIM_SR_UIF)==0){} TIM3->SR &= ~TIM_SR_UIF;}I did some changes and works fine now , but i can't understand why it didn't work the previous version .2013-02-22 10:24 AM
void Delay_ms(uint16_t ms)
{
uint16_t start = TIM3->CNT; // assumes struct is volatile
while((TIM3->CNT - start) < ms);
} Arguably a better solution would be to meter in micro seconds, and have a smaller prescaler.
2013-03-01 12:18 PM
This delay function needs to take care of the case when there is an overflow in the counter, i.e., TIM3->CNT wraps around.
2013-03-01 1:09 PM
This delay function needs to take care of the case when there is an overflow in the counter, i.e., TIM3->CNT wraps around.
Actually it does. It might have issues if you exceed the scope (ie >65.535 Seconds), but is otherwise sound.We’re moving the ST Community to a new platform to give you a better and more reliable community experience.