2012-09-14 08:49 AM
Hi,
I have a new board based on STM32F407 that is wired iin RMII with a KSZ8031RNL PHY. I would like to port the stm32 f4 eval board sample to my board. I have defined the RMII_MODEHere the maping of the phy ETH_MDIO -------------------------> PA2 ETH_MDC --------------------------> PC1 ETH_MII_RX_CLK/ETH_RMII_REF_CLK---> PA1 ETH_MII_RX_DV/ETH_RMII_CRS_DV ----> PA7 ETH_MII_RXD0/ETH_RMII_RXD0 -------> PC4 ETH_MII_RXD1/ETH_RMII_RXD1 -------> PC5 ETH_MII_TX_EN/ETH_RMII_TX_EN -----> PB11 ETH_MII_TXD0/ETH_RMII_TXD0 -------> PB12 ETH_MII_TXD1/ETH_RMII_TXD1 -------> PB13I have change the GPIO init to /* Configure PA1, PA2 and PA7 */ GPIO_InitStructure.GPIO_Pin = GPIO_Pin_1 | GPIO_Pin_2 | GPIO_Pin_7; GPIO_Init(GPIOA, &GPIO_InitStructure); GPIO_PinAFConfig(GPIOA, GPIO_PinSource1, GPIO_AF_ETH); GPIO_PinAFConfig(GPIOA, GPIO_PinSource2, GPIO_AF_ETH); GPIO_PinAFConfig(GPIOA, GPIO_PinSource7, GPIO_AF_ETH); /* Configure PC1, PC4 and PC5 */ GPIO_InitStructure.GPIO_Pin = GPIO_Pin_1 | GPIO_Pin_4 | GPIO_Pin_5; GPIO_Init(GPIOC, &GPIO_InitStructure); GPIO_PinAFConfig(GPIOC, GPIO_PinSource1, GPIO_AF_ETH); GPIO_PinAFConfig(GPIOC, GPIO_PinSource4, GPIO_AF_ETH); GPIO_PinAFConfig(GPIOC, GPIO_PinSource5, GPIO_AF_ETH); /* Configure PB11, PB12 and PB13 */ GPIO_InitStructure.GPIO_Pin = GPIO_Pin_11 | GPIO_Pin_12 | GPIO_Pin_13; GPIO_Init(GPIOB, &GPIO_InitStructure); GPIO_PinAFConfig(GPIOB, GPIO_PinSource11, GPIO_AF_ETH); GPIO_PinAFConfig(GPIOB, GPIO_PinSource12, GPIO_AF_ETH); GPIO_PinAFConfig(GPIOB, GPIO_PinSource13, GPIO_AF_ETH);here my part of bsp initvoid ETH_BSP_Config(void){ /* Configure the GPIO ports for ethernet pins */ ETH_GPIO_Config(); /* Config NVIC for Ethernet */ ETH_NVIC_Config(); /* Configure the Ethernet MAC/DMA */ ETH_MACDMA_Config();}In the ETH_MACDMA_Config /* Reset ETHERNET on AHB Bus */ ETH_DeInit(); /* Software reset */ ETH_SoftwareReset(); /* Wait for software reset */ while (ETH_GetSoftwareResetStatus() == SET); /* Enable ETHERNET clock */ RCC_AHB1PeriphClockCmd(RCC_AHB1Periph_ETH_MAC | RCC_AHB1Periph_ETH_MAC_Tx | RCC_AHB1Periph_ETH_MAC_Rx, ENABLE);.......}If i put the RCC_AHB1PeriphClockCmd before the while (ETH_GetSoftwareResetStatus() == SET); I loop there foreever. I see somewhere in this forum That the MAC clock sould not be anabled before reseting it. I don't know why this is done in the ST sample. Now in the ETH_Init I always loop here if(ETH_InitStruct->ETH_AutoNegotiation != ETH_AutoNegotiation_Disable) { /* We wait for linked status... */ do { timeout++; } while (!(ETH_ReadPHYRegister(PHYAddress, PHY_BSR) & PHY_Linked_Status) && (timeout < PHY_READ_TO));}
I have change the PHYAddress to fit with the real PHY (0x00).I try to debug this. This is the first time I debug a PHY !!!I have looked at some pin With the SCOPE and I can confirm this.I have a 50Mhz clock on the Clk_ref pin. When a packed is received from the network (normal traffic) I see the RDX0 and RXD1 moving. But When I look at RMII_TX_EN and RMII_TXD0 and RMII_TX1, nothing change on thoses pin. It look like this pin is tied to low. I'm probably missing something there. For Now I have no idea what !Is there a technic (like a step by step) to debug this thing ?regardsJonathan2012-12-20 06:41 AM
Hi Jonathan,
Im facing exactly the same issue and I'm very new to ethernet debugging. Were you able to find the issue that you have mentioned ????2012-12-20 06:48 AM
Just to add to above point, I'm able to read the basic control and status registers properly so it looks like im able to communicate with the PHY. But the link status bit is always ZERO (link is down).
2013-09-02 09:00 PM
I am porting an ethernet application from a Keil board MCBSTM32F100 to an MCBSTM32F200 board. I have everything working but the ethernet port. Using the migration document I reconfigured all the GPIO pins and clock initializations. I still can't get the port to work. I tried everything I could think of but had no luck. I am looking for code example oe an App Note. Can anyone help me with this.