Dead time generation STM32F030K6
Options
- Mark as New
- Bookmark
- Subscribe
- Mute
- Subscribe to RSS Feed
- Permalink
- Email to a Friend
- Report Inappropriate Content
‎2014-02-15 12:53 PM
Posted on February 15, 2014 at 21:53
This software is not working with STM32F030K6 , but this sofware works with STM32F030R8. Prototype 1 used the discovery board. No we made a PCB with
STM32F030K6. And the code is not working anymore. Makes reset. If I don't call this routine, then the softtware is working also on STM32F030K6. But then we don't have the brushless sensorless functionality. Is any work arround possible. I have a 3 phase brushless motor. For the operation I need a very low cost non overlapping PWM unit. The software use only TIM1. So I can not understand why the software is not working with the smaller member STM32F030K6. (TIM15/16/17 is not used in this sample) ) ** ****************************************************************************** * @file Spwm.c * @author MCD Application Team * @version V1.0.0 * @date 16.1.2014 * @brief Tim1 3 Phase PWM for block commutation sensorless ****************************************************************************** * * ****************************************************************************** */ /* Includes ------------------------------------------------------------------*/ &sharpinclude ''pwm.h'' &sharpinclude ''stm32f0xx.h'' &sharpinclude ''stm32f0xx_tim.h'' //&sharpinclude ''stm32f0xx_gpio.h'' //&sharpinclude ''stm32f0xx_rcc.h'' /* Private variables ---------------------------------------------------------*/ //uint16_t Channel1Pulse = 0, Channel2Pulse = 0, Channel3Pulse = 0; TIM_TimeBaseInitTypeDef TIM_TimeBaseStructure; TIM_OCInitTypeDef TIM_OCInitStructure; TIM_BDTRInitTypeDef TIM_BDTRInitStructure; uint16_t TimerPeriod = 0; //uint16_t Channel1Pulse = 0, Channel2Pulse = 0, Channel3Pulse = 0; /* Private function prototypes -----------------------------------------------*/ /** * @brief Main program. * @param None * @retval None */ void Complementary_signals(void) { &sharpdefine PWM_FREQ 100000 TimerPeriod = (SystemCoreClock / PWM_FREQ); //16kHz TimerPeriod = 3000 TIM_TimeBaseStructInit(&TIM_TimeBaseStructure); /* Time Base configuration */ TIM_TimeBaseStructure.TIM_Prescaler = 0; TIM_TimeBaseStructure.TIM_CounterMode = TIM_CounterMode_Up; TIM_TimeBaseStructure.TIM_Period = TimerPeriod; TIM_TimeBaseStructure.TIM_ClockDivision = 0; TIM_TimeBaseStructure.TIM_RepetitionCounter = 0; TIM_TimeBaseInit(TIM1, &TIM_TimeBaseStructure); /* Channel 1, 2 and 3 Configuration in PWM mode */ TIM_OCInitStructure.TIM_OCMode = TIM_OCMode_PWM2; TIM_OCInitStructure.TIM_OutputState = TIM_OutputState_Enable; TIM_OCInitStructure.TIM_OutputNState = TIM_OutputNState_Enable; TIM_OCInitStructure.TIM_Pulse = 0; TIM_OCInitStructure.TIM_OCPolarity = TIM_OCPolarity_High; TIM_OCInitStructure.TIM_OCNPolarity = TIM_OCNPolarity_High; TIM_OCInitStructure.TIM_OCIdleState = TIM_OCIdleState_Set; TIM_OCInitStructure.TIM_OCNIdleState = TIM_OCIdleState_Reset; TIM_OC1Init(TIM1, &TIM_OCInitStructure); TIM_OCInitStructure.TIM_Pulse = 0; TIM_OC2Init(TIM1, &TIM_OCInitStructure); TIM_OCInitStructure.TIM_Pulse = 0; TIM_OC3Init(TIM1, &TIM_OCInitStructure); /* Automatic Output enable, Break, dead time and lock configuration*/ TIM_BDTRInitStructure.TIM_OSSRState = TIM_OSSRState_Enable; TIM_BDTRInitStructure.TIM_OSSIState = TIM_OSSIState_Enable; TIM_BDTRInitStructure.TIM_LOCKLevel = TIM_LOCKLevel_1; TIM_BDTRInitStructure.TIM_DeadTime = 20; TIM_BDTRInitStructure.TIM_Break = TIM_Break_Enable; TIM_BDTRInitStructure.TIM_BreakPolarity = TIM_BreakPolarity_High; TIM_BDTRInitStructure.TIM_AutomaticOutput = TIM_AutomaticOutput_Enable; TIM_BDTRConfig(TIM1, &TIM_BDTRInitStructure); /* TIM2 TRGO selection */ TIM_SelectOutputTrigger(TIM1, TIM_TRGOSource_Update); // ADC_ExternalTrigConv_T2_TRGO /* TIM1 counter enable */ TIM_Cmd(TIM1, ENABLE); /* Main Output Enable */ TIM_CtrlPWMOutputs(TIM1, ENABLE); } Franz #stm32f030k6-dead-time-with-tim1
Labels:
- Labels:
-
TIM
This discussion is locked. Please start a new topic to ask your question.
2 REPLIES 2
Options
- Mark as New
- Bookmark
- Subscribe
- Mute
- Subscribe to RSS Feed
- Permalink
- Email to a Friend
- Report Inappropriate Content
‎2014-02-15 3:24 PM
Posted on February 16, 2014 at 00:24
It's physically resetting the part? Then you're going to have to look at the supplies, the power routing, bulk capacitance, and shorted pins.
Tips, Buy me a coffee, or three.. PayPal Venmo
Up vote any posts that you find helpful, it shows what's working..
Up vote any posts that you find helpful, it shows what's working..
Options
- Mark as New
- Bookmark
- Subscribe
- Mute
- Subscribe to RSS Feed
- Permalink
- Email to a Friend
- Report Inappropriate Content
‎2014-02-17 12:18 PM
Posted on February 17, 2014 at 21:18
Thank you. It was an hardware problem. Now it works.