DAC specification 8-10bit mode?
Options
- Mark as New
- Bookmark
- Subscribe
- Mute
- Subscribe to RSS Feed
- Permalink
- Email to a Friend
- Report Inappropriate Content
2017-10-03 7:21 PM
Posted on October 04, 2017 at 04:21
STM32F4xx
1: Do 8bit DAC mode have same specifications as the 10bit mode?
2: The 3.3V / 1.5MOhm = 2.2 µA load for 1% accuracy as spec'ed in manual is for internal
buffer off , i had assumed no load at all would give best accuracy when using non inverting external buffers? No?
This discussion is locked. Please start a new topic to ask your question.
0 REPLIES 0