Posted on October 04, 2017 at 06:13I have read the previous post on why the Inventek module was used instead of the SPWF04SA on STM32L4 IoT Discovery kit. My understanding is that ST recommends using the SPWF04SA going forward. Is this correct?I I would like to try replacing Inventek module with SPWF04SA on STM32L4 Discovery kit IoT node using X-NUCLEO-IDW04A1 expansion board with SPI by changing the port pins and setting the flag for SPI. Is the WiFi protocol over SPI the same for the Inventek module as the SPWF04SA module or do I need to use software from the SPWF01 module?