cancel
Showing results for 
Search instead for 
Did you mean: 

custom board support interface Creation

ygrod
Associate II
Posted on December 13, 2016 at 08:39

Hi. Can't find at uVision5 how to create custom board support interface for 'New Project'...... Thanks in advance

This discussion is locked. Please start a new topic to ask your question.
3 REPLIES 3
Lawliet KG
Associate III
Posted on December 13, 2016 at 12:44

Hi

Grodetsky.Yury

,

If you will use

uVision5

, there is no need to

create a custom board support interface, you can simply:

  • Select the device that you will work with.

-> 'Manage Run-Time Environment' window will appear.

  • In section 'Board support', you will get a list of the available boards using the

    chosen

    MCU.
  • Selectthe convenient board.

If this answers your request, please press 'correct'

:)

.

Regards,

Lawliet.

Posted on December 13, 2016 at 13:33

thanks, but i imply inclusion of support for my own hardware.......

Lawliet KG
Associate III
Posted on December 14, 2016 at 14:12

Hi

Grodetsky.Yury

,

I advise you to use SW4STM32 IDE. It gives you the ability to create your own custom board.

Regards,

Lawliet.