cancel
Showing results for 
Search instead for 
Did you mean: 

CubeMX v4.26 CubeH7 TIM1/8. Where are CH5/6?

Grisby
Associate II
Posted on June 29, 2018 at 15:16

I have read RM0433 and DS12110 . TIM1/8 has 4 Channel. But in CubeMX v4.26 I can see 6 Channel in CubeH7 v1.2.0.

Is this a bug?

#stm32h7
This discussion is locked. Please start a new topic to ask your question.
1 REPLY 1
Imen.D
ST Employee
Posted on June 29, 2018 at 18:48

Hello

Belter.Chris

 ,

The STM32H7 reference manual and datasheet mentioned that there is 6 channels for TIM1 and TIM8.

For example for TIM1, they have these channels:

TIM1_CH1,  

TIM1_CH2,  

TIM1_CH3 with 

three complementary channels: 

TIM1_CH1N,  

TIM1_CH2N,  

TIM1_CH3N.

0690X0000060LUaQAM.png

With Regards,

Imen.

When your question is answered, please close this topic by clicking "Accept as Solution".
Thanks
Imen