Skip to main content
Ahmed Elzoughby
Associate II
June 24, 2018
Solved

Relocating Vector Table to AXISRAM in STM32H743

  • June 24, 2018
  • 12 replies
  • 4090 views
Posted on June 24, 2018 at 13:03

Hi,

I am using the Nucleo-H743ZI development board and trying to make an Interrupt driver for it. The driver has to support changing the vector table contents at runtime. So I made a copy of the vector table in the AXI SRAM at its first address (0x24000000)

typedef void(*voidPFn_t)(void);

static volatile voidPFn_t newVectorTable[_VECTOR_TABLE_SIZE] __attribute__ ((section('.sram_d1')));

void interruptInit() {

    volatile voidPFn_t* origVectorTable = (voidPFn_t*) SCB->VTOR;

    // copy the content of the original vector table into the new vector table

    for(uint32_t i = 0; i < _VECTOR_TABLE_SIZE; i++)

        newVectorTable[i] = origVectorTable[i];

    // install the new interrupt vector table

    SCB->VTOR = ((uint32_t) &newVectorTable);

}

I succeeded to copy the content of the original vector table and I could see that through the memory window of my IDE. Also I set the VTOR register to 0x24000000 and modified my new vector table correctly.

But the problem is when I fire an interrupt in my test example the cpu goes to execute the interrupt handler of the original vector table not my new vector table. I don't know why that happens.

#interrupt #stm32h743 #nucleo-h743zi #stm32h7 #vector-table #axi-sram
This topic has been closed for replies.
Best answer by Abdelhamid GHITH
Posted on June 27, 2018 at 14:17

Hi!

I think you are facing a cache coherency issue (

https://www.st.com/content/ccc/resource/technical/document/application_note/group0/08/dd/25/9c/4d/83/43/12/DM00272913/files/DM00272913.pdf/jcr:content/translations/en.DM00272913.pdf

for some details about cache & cache coherency).

newVectorTable[VECSYSTICK] = &SysTick_Handler_New; // SysTick Handler

/* perform a cache maintenance : can be optimized by using SCB_CleanDCache_by_Addr  */

SCB_CleanDCache();

SCB_InvalidateICache();

Br,

Abdel

12 replies

Tesla DeLorean
Guru
June 24, 2018
Posted on June 24, 2018 at 17:30

Suggest using the ITCM RAM at 0x00000000

Tips, Buy me a coffee, or three.. PayPal Venmo (See Profile) Up vote any posts that you find helpful, it shows what's working..
Ahmed Elzoughby
Associate II
June 24, 2018
Posted on June 24, 2018 at 21:49

Tried that, but nothing new. the same problem occurred.

Tesla DeLorean
Guru
June 24, 2018
Posted on June 24, 2018 at 23:04

I've tried relocating the vector table on an STM32H743I-EVAL, reasonably standard configuration, with caching enabled.

I can copy the vectors to ITCM RAM, and change the SysTick_Handler routine to point to another one, which outputs periodically so I can see it is using that one, and not the standard one.

void SysTick_Handler_New(void)

{

    static int i = 0;

    

    if (i == 0) putchar('*');

    i = (i + 1) % 1000;

    

  HAL_IncTick();

}

...

♯ define VECSYSTICK 15

...

newVectorTable[VECSYSTICK] = &SysTick_Handler_New; // SysTick Handler

I can see it transition to the newly pointed too code.

If I use AXI SRAM it vectors off some illegal address

Tips, Buy me a coffee, or three.. PayPal Venmo (See Profile) Up vote any posts that you find helpful, it shows what's working..
Abdelhamid GHITH
Abdelhamid GHITHBest answer
ST Employee
June 27, 2018
Posted on June 27, 2018 at 14:17

Hi!

I think you are facing a cache coherency issue (

https://www.st.com/content/ccc/resource/technical/document/application_note/group0/08/dd/25/9c/4d/83/43/12/DM00272913/files/DM00272913.pdf/jcr:content/translations/en.DM00272913.pdf

for some details about cache & cache coherency).

newVectorTable[VECSYSTICK] = &SysTick_Handler_New; // SysTick Handler

/* perform a cache maintenance : can be optimized by using SCB_CleanDCache_by_Addr  */

SCB_CleanDCache();

SCB_InvalidateICache();

Br,

Abdel

Tesla DeLorean
Guru
June 27, 2018
Posted on June 27, 2018 at 17:20

Had tried SCB_InvalidateDCache_by_Addr(), working today. Evidence suggests no write-through/invalidation occurs on the I-Cache normally, ggrr!

Tips, Buy me a coffee, or three.. PayPal Venmo (See Profile) Up vote any posts that you find helpful, it shows what's working..
Tesla DeLorean
Guru
June 29, 2018
Posted on June 29, 2018 at 03:18

Ok, so having cycled the power on the STM32H743I-EVAL, changing the RAM at 0x24000000, resulted in the failure of SCB_InvalidateDCache_by_Addr() to achieve the goal, and the SysTick vectors off to some to some random junk.

SCB_InvalidateDCache_by_Addr((uint32_t*)newVectorTable, VECSIZE);

Tips, Buy me a coffee, or three.. PayPal Venmo (See Profile) Up vote any posts that you find helpful, it shows what's working..
Vitaliy Kostyrev
Associate
June 29, 2018
Posted on June 29, 2018 at 04:10

extern

uint32_t __Vectors[];

/* vector table ROM */

#define VECTORTABLE_SIZE (256)

/* size Cortex-M7 vector table */

#define VECTORTABLE_ALIGNMENT (0x100ul) 

#define ADDRESS_SRAM *(uint32_t*)0x2400000

#define NEXT_ADDRESS_SRAM(A) (ADDRESS_SRAM+(A))

/* next power of 2 = 256 */

/* new vector table in RAM */

uint32_t vectorTable_RAM[VECTORTABLE_SIZE] __attribute__(( aligned (VECTORTABLE_ALIGNMENT) ));

/*----------------------------------------------------------------------------

SysTick_Handler

*----------------------------------------------------------------------------*/

volatile

uint32_t msTicks = 0;

/* counts 1ms timeTicks */

void

SysTick_Handler(

void

) {

msTicks++;

/* increment counter */

}

/*----------------------------------------------------------------------------

SysTick_Handler (RAM)

*----------------------------------------------------------------------------*/

volatile

uint32_t msTicks_RAM = 0;

/* counts 1ms timeTicks */

void

SysTick_Handler_RAM(

void

) {

msTicks_RAM++;

/* increment counter */

}

/*----------------------------------------------------------------------------

MAIN function

*----------------------------------------------------------------------------*/

int

main (

void

) {

uint32_t i;

for

(i = 0; i < VECTORTABLE_SIZE; i++) {

NEXT_ADDRESS_SRAM(i)

= __Vectors[i];

/* copy vector table to RAM */

}

/* replace SysTick Handler */

NEXT_ADDRESS_SRAM

[

http://www.keil.com/pack/doc/CMSIS/Core/html/group__NVIC__gr.html#gga7e1129cd8a196f4284d41db3e82ad5c8a6dbff8f8543325f3474cbae2446776e7

+ 16] = (uint32_t)SysTick_Handler_RAM;

/* relocate vector table */

http://www.keil.com/pack/doc/CMSIS/Core/html/group__Core__Register__gr.html#gaeb8e5f7564a8ea23678fe3c987b04013

();

SCB->VTOR = (uint32_t)&vectorTable_RAM;

http://www.keil.com/pack/doc/CMSIS/Core/html/group__intrinsic__CPU__gr.html#gacb2a8ca6eae1ba4b31161578b720c199

();

http://www.keil.com/pack/doc/CMSIS/Core/html/group__Core__Register__gr.html#ga0f98dfbd252b89d12564472dbeba9c27

();

http://www.keil.com/pack/doc/CMSIS/Core/html/group__system__init__gr.html#gae0c36a9591fe6e9c45ecb21a794f0f0f

();

/* Get Core Clock Frequency */

http://www.keil.com/pack/doc/CMSIS/Core/html/group__SysTick__gr.html#gabe47de40e9b0ad465b752297a9d9f427

(

http://www.keil.com/pack/doc/CMSIS/Core/html/group__system__init__gr.html#gaa3cd3e43291e81e795d642b79b6088e6

/ 1000ul);

/* Setup SysTick Timer for 1 msec */

while

(1);

}

Vitaliy Kostyrev
Associate
June 29, 2018
Posted on June 29, 2018 at 04:12

SCB-> VTOR = (uint32_t) &

ADDRESS_SRAM

;