cancel
Showing results for 
Search instead for 
Did you mean: 

CubeMX '': is an invalid character in resource name 'virtual:'.''

smhhadima
Associate II
Posted on May 20, 2016 at 20:54

After I upgraded to CubeMX 4.14.0, I got this error at ''TrueSTUDIO'' once I created a new project:

'': is an invalid character in resource name 'virtual:'.''

the previous version works fine but the new update generate such error.

How can I solve the issue?
This discussion is locked. Please start a new topic to ask your question.
4 REPLIES 4
Nesrine M_O
Lead II
Posted on May 23, 2016 at 19:12

Hi SamTheMan,

I'll report this issue to our MX team for checking. Sorry for the inconvenience it may bring.

-Syrine-

stm32cube-t
ST Employee
Posted on May 24, 2016 at 10:34

Dear user,

Please upgrade to latest CubeMX 4.15 release as 4.14 revealed several issues with TrueStudio support.

If you encounter the issue again, please indicate on which OS you are working and provide  us with the STM32CubeMX configuration file (.ioc file) of your project.

Thanks
smhhadima
Associate II
Posted on May 26, 2016 at 12:57

The original post was too long to process during our migration. Please click on the provided URL to read the original post. https://st--c.eu10.content.force.com/sfc/dist/version/download/?oid=00Db0000000YtG6&ids=0680X000006I6Vz&d=%2Fa%2F0X0000000bpe%2FZE3FZFmSu8c52QoavFRP80yTZZIq6a7MsWbX9LX.Mg0&asPdf=false
smhhadima
Associate II
Posted on May 26, 2016 at 14:14

it seems like the .ioc files that was generated by version 4.14 is NOT compatible with 4.15 version!

because the above problem keeps happening with .ioc files that was generated originally with cube 4.14 (although I did the migration to 4.15)