cancel
Showing results for 
Search instead for 
Did you mean: 

CubeMX Feature Request: Add CAN TTrig Functionality

Ed Maynard
Associate II
Posted on October 26, 2017 at 18:54

I would be nice to have access to the timing features present when using Time-Triggered Mode on the CAN modules. Specifically the RDTR and TDTR registers. Additionally, why not simply make copies of the registers available in the register structure definition. The issue is that trying to read the contents AFTER the mailbox has been released yields garbage.

This discussion is locked. Please start a new topic to ask your question.
0 REPLIES 0