2015-09-23 01:15 AM
Hello,
i have a serious problem with project regeneration with CubeMX. After regenerating a project, the linked files (for example HAL and configuration files, like main.c) point to the wrong direction. The file links still has the right name (''adc.c'' but points to/opens a wrong file (for example, all file links generated by CubeMX point to the first file found, like adc.c or startup_stm32f746xx.s. This is very annoying. Is this a known bug? Any workaround besides deleting the project and adding custom libs/includes every time?2015-09-23 03:51 AM
It seems this is the wrong Category of the community board, i created a new thread here:
https://my.st.com/public/STe2ecommunities/mcu/Lists/STM32Java/Flat.aspx?RootFolder=%2fpublic%2fSTe2ecommunities%2fmcu%2fLists%2fSTM32Java%2fBug%20Report%20CubeMX%20Corrupts%20File%20Links%20in%20OpenSTM32&FolderCTID=0x01200200770978C69A1141439FE559EB459D758000F9A0E3A95BA69146A17C2E80209ADC21&TopicsV...