cancel
Showing results for 
Search instead for 
Did you mean: 

CubeMX Code Generation Issue for STM32L1 Parts

dpryan
Associate II
Posted on April 11, 2016 at 22:31

CubeMX thinks there is a ''FW.L1.1.1.5.0'' update for the STM32L1 parts.

However, it cannot download the update (''Not yet available'').

When I download manually from the website, it seems like the cube software is only v1.4 (despite the download link claiming to be v1.5).

I can't get CubeMX to generate code with this issue (even with v1.4 installed).

This discussion is locked. Please start a new topic to ask your question.
3 REPLIES 3
slimen
Senior
dpryan
Associate II
Posted on April 12, 2016 at 22:10

Thanks. The manual update using your link worked!

I was already using the latest version of CubeMX, so there's still a problem with the automatic update for that L1 library.

Previously, when I tried the manual update, but I was using a different link (http://www.st.com/web/en/catalog/tools/PF260821). Even though that website says v1.5, when you download it, it is actually v1.4.

slimen
Senior
Posted on April 13, 2016 at 11:22

Hi ryan,

I have downloaded v1.5 though the same website  http://www.st.com/web/en/catalog/tools/PF260821 and I have the package installed STM32Cube_FW_L1_V1.5.0

Regards