Skip to main content
Rudas.Robert
Associate II
August 12, 2016
Question

CubeMX and repository examples

  • August 12, 2016
  • 3 replies
  • 833 views
Posted on August 13, 2016 at 00:31

Hi,

I'm new to programming the STM32 micro. That's way the Cubemx tool is very helpful for initializing the STM32. Also ther are a lot of examples in the repository, but i don't understand why the examples are not writen in CubeMX if there are provided with the tool?

The tool save me a lot of time for initializing, but i spend a lot of time to figure out how is the correct usage of initialized files (functions), and import the provided example in repository to CubeMX generated project.
    This topic has been closed for replies.

    3 replies

    LMI2
    Senior III
    August 14, 2016
    Posted on August 14, 2016 at 18:28

    The Idea of STM32CubeMX is very good in my opinion. But the tool itself is not finished (yet?). Even ST itself is not using it in their examples. About that there has been several comments in this forum.

    I have used blocking ADC and blocking serial io functions from Cube. They were easy enough that I could do it just by guessing.

    Walid FTITI_O
    Visitor II
    August 15, 2016
    Posted on August 15, 2016 at 17:53

    Hi kolja111

    ,

    Note that , STM32CubeMX is a graphical interface which  performs the following functions:

    • Fast and easy configuration of the MCU pins, clock tree and operating modes for the selected peripherals and middleware

    • Generation of pin configuration report for board designers

    ʉۢ Generation of a complete project with all the necessary libraries and initialization C code to set up the device in the user defined operating mode.

    Thus, The project generated is an initialization project

     used as base for the user's application and can be directly open in the selected application development environment (for a selection of supported IDEs) to proceed with application development.

    For the library examples, there is a plan in the future to give the ''.ioc'' files used for Initialization.

    -Hannibal-

    Rudas.Robert
    Associate II
    August 16, 2016
    Posted on August 16, 2016 at 13:41

    Hi,

    the usage of CubeMx is easy understandable for me. But it would be nice, to see the proper usage of functions, generated from the tool and which function do i have to call. So it would be great that the examples are made in CubeMX generated files.

    I do not expect that ST updates the examples for all developmen boards but only the newest like STML4 and STM32F7, that have been introduced long after the CubeMX tool.