CUBEMX ADC
Options
- Mark as New
- Bookmark
- Subscribe
- Mute
- Subscribe to RSS Feed
- Permalink
- Email to a Friend
- Report Inappropriate Content
‎2016-05-23 2:14 PM
Posted on May 23, 2016 at 23:14
Hi,
I have started to work with STM32L1. Maybe it's a silly questestion, but how to read multiple ADC channels without DMA? It is simple to read 1 channel with HAL_ADC_GetValue(&hadc); or multiple channels with DMA HAL_ADC_Start_DMA(&hadc, advalues, 3);
/* ADC init function */
void MX_ADC_Init(void)
{
ADC_ChannelConfTypeDef sConfig;
/**Configure the global features of the ADC (Clock, Resolution, Data Alignment and number of conversion)
*/
hadc.Instance = ADC1;
hadc.Init.ClockPrescaler = ADC_CLOCK_ASYNC_DIV1;
hadc.Init.Resolution = ADC_RESOLUTION12b;
hadc.Init.DataAlign = ADC_DATAALIGN_RIGHT;
hadc.Init.ScanConvMode = ADC_SCAN_DISABLE;
hadc.Init.EOCSelection = EOC_SEQ_CONV;
hadc.Init.LowPowerAutoWait = ADC_AUTOWAIT_DISABLE;
hadc.Init.LowPowerAutoPowerOff = ADC_AUTOPOWEROFF_DISABLE;
hadc.Init.ChannelsBank = ADC_CHANNELS_BANK_A;
hadc.Init.ContinuousConvMode = DISABLE;
hadc.Init.NbrOfConversion = 3;
hadc.Init.DiscontinuousConvMode = DISABLE;
hadc.Init.ExternalTrigConv = ADC_SOFTWARE_START;
hadc.Init.ExternalTrigConvEdge = ADC_EXTERNALTRIGCONVEDGE_NONE;
hadc.Init.DMAContinuousRequests = DISABLE;
HAL_ADC_Init(&hadc);
/**Configure for the selected ADC regular channel its corresponding rank in the sequencer and its sample time.
*/
sConfig.Channel = ADC_CHANNEL_11;
sConfig.Rank = 1;
sConfig.SamplingTime = ADC_SAMPLETIME_4CYCLES;
HAL_ADC_ConfigChannel(&hadc, &sConfig);
/**Configure for the selected ADC regular channel its corresponding rank in the sequencer and its sample time.
*/
sConfig.Channel = ADC_CHANNEL_12;
sConfig.Rank = 2;
HAL_ADC_ConfigChannel(&hadc1, &sConfig);
/**Configure for the selected ADC regular channel its corresponding rank in the sequencer and its sample time.
*/
sConfig.Channel = ADC_CHANNEL_13;
sConfig.Rank = 3;
HAL_ADC_ConfigChannel(&hadc, &sConfig);
}
2 REPLIES 2
Options
- Mark as New
- Bookmark
- Subscribe
- Mute
- Subscribe to RSS Feed
- Permalink
- Email to a Friend
- Report Inappropriate Content
‎2016-05-23 5:16 PM
Posted on May 24, 2016 at 02:16
how to read multiple ADC channels without DMA?
You could use different ADC? The STM32 model is to use DMA so there isn't a lot of wasted time reconfiguring, looping, and the measurements can be serviced in a HT/TC interrupt.
Tips, Buy me a coffee, or three.. PayPal Venmo
Up vote any posts that you find helpful, it shows what's working..
Up vote any posts that you find helpful, it shows what's working..
Options
- Mark as New
- Bookmark
- Subscribe
- Mute
- Subscribe to RSS Feed
- Permalink
- Email to a Friend
- Report Inappropriate Content
‎2016-05-24 7:08 AM
Posted on May 24, 2016 at 16:08
This is the procedure:
- Configure the ADC so that a scan conversion is performed (hadc.Init.ScanConvMode = ADC_SCAN_ENABLE).
- Set EOC to end of each conversion rank (hadc.Init.EOCSelection = ADC_EOC_SINGLE_CONV).
- Configure channels.
- Start conversions using HAL_ADC_Start();
- Poll for each conversion using HAL_ADC_PollForConversion().
- Get the conversion result using HAL_ADC_GetValue().
IMHO, performing scan conversion using DMA is the best option.