cancel
Showing results for 
Search instead for 
Did you mean: 

CubeMX 4.12.0 Bug Report

misagh
Associate III
Posted on January 24, 2016 at 08:27

Hello everybody,

When I use FreeRTOS, the cubemx generates following code for

SysTick_Handler()

:

void SysTick_Handler(void)

{

  /* USER CODE BEGIN SysTick_IRQn 0 */

  /* USER CODE END SysTick_IRQn 0 */

  osSystickHandler();

  /* USER CODE BEGIN SysTick_IRQn 1 */

   

  /* USER CODE END SysTick_IRQn 1 */

}

Therefore,

HAL_Delay()

doesn't work. When we use LSI, HAL library will call

HAL_Delay(1)

function while initializing clock in

 SystemClock_Config()

and the program will go to infinite loop.

So I added this code to

SysTick_Handler()

:

void SysTick_Handler(void)

{

  /* USER CODE BEGIN SysTick_IRQn 0 */

  /* USER CODE END SysTick_IRQn 0 */

  osSystickHandler();

  /* USER CODE BEGIN SysTick_IRQn 1 */

    HAL_IncTick();

  /* USER CODE END SysTick_IRQn 1 */

}

I hope this problem solve in next CubeMX versions.

Bests,

Misagh

This discussion is locked. Please start a new topic to ask your question.
3 REPLIES 3
laurentschroeder
Associate
Posted on January 24, 2016 at 13:30

I am having the exact same issue. But I am surprised that the removal of HAL_IncTick() is intentional as described in the release notes of STM32CubeMX V4.12.0: ''[MX-FreeRTOS/NVIC] HAL_IncTick must be removed and systick prio must be the lowest

 

when FreeRTOS is activated''

So what would be the correct way to implement the SysTick_Handler?
Nesrine M_O
Lead II
Posted on January 25, 2016 at 11:25

Hi,

Thank you for your feedback. The issue is already tracked and reported internally.

-Syrine-

stm32cube-t
ST Employee
Posted on January 25, 2016 at 19:15

Dear user,

This is an issue.

Also, for configurations using freeRTOS, the user shall systematically change the default HAL time-base (systick) to an hardware time-base.

HAL time base relative functions are weak to allow the user to select another hardware time-base.

In next CubeMX 4.13 version, under the SYS peripheral, it will be possible to select a different timing source for the HAL (tim1, tim2, rtc,...) and automatically generate the functions overloading the weak HAL time base relative functions.

This way, RTOS and HAL time-base will be completely disassociated.

Note also, that user code placed in the HAL user callbacks should use safe FreeRTOS APIs only. Best regards