Question
Cube MX configures MISO and MOSI as outputs in SPI Full Duplex Master
Posted on February 26, 2018 at 11:43
I am using an STM32L031K6 and I configure SP1 as Full Duplex Master, I expect that MOSI is an output and MISO an input but Cube MX configures SPI1_MISO as a Alternate Function Push Pull and can not be changed.
If I short MISO and MOSI of course doesn't work because both are outputs.
Why is it like that?
Thanks.