Crystal selection guide
- Mark as New
- Bookmark
- Subscribe
- Mute
- Subscribe to RSS Feed
- Permalink
- Email to a Friend
- Report Inappropriate Content
‎2024-12-31 3:01 AM
- Mark as New
- Bookmark
- Subscribe
- Mute
- Subscribe to RSS Feed
- Permalink
- Email to a Friend
- Report Inappropriate Content
‎2024-12-31 3:17 AM - edited ‎2024-12-31 3:33 AM
Hello @parth4 and welcome to the ST Community.
I advise you to refer to this AN2867 Application note "Oscillator design guide for STM8AF/AL/S, STM32 MCUs and MPUs" and check the Table 6 and 7 for recommended crystal, that may help you on your needs.
Best Regards.
STTwo-32
To give better visibility on the answered topics, please click on Accept as Solution on the reply which solved your issue or answered your question.
- Mark as New
- Bookmark
- Subscribe
- Mute
- Subscribe to RSS Feed
- Permalink
- Email to a Friend
- Report Inappropriate Content
‎2024-12-31 3:29 AM
THERE IS NO SPECIFICATION ABOUT 8MHZ CRYSTAL COMPONENT FOR STM32L4 SERIES , IN TABLE 7 THERE IS ONLY 32.768KHZ CRYSTAL ARE THERE BECAUSE IT IS LSE TABLE, SHARE THE PART NUMBER IF YOU CAN OTHERWISE GUIDE US FOR SELECTION PARAMETER LIKE CAPACITANCE LOAD, FREQUENCY TOLERANCE.
- Mark as New
- Bookmark
- Subscribe
- Mute
- Subscribe to RSS Feed
- Permalink
- Email to a Friend
- Report Inappropriate Content
‎2024-12-31 3:40 AM
Please have a look at the chapters 4 and 5. You should have a guide on how to select your oscilator for both LSE and HSE.
Best Regard.
STTwo-32
To give better visibility on the answered topics, please click on Accept as Solution on the reply which solved your issue or answered your question.
- Mark as New
- Bookmark
- Subscribe
- Mute
- Subscribe to RSS Feed
- Permalink
- Email to a Friend
- Report Inappropriate Content
‎2024-12-31 4:14 AM
CAN YOU PLEASE GIVE ME VALUE OF LOAD CAPACITANCE OF 8 MHZ CRYSTAL FOR STM32L462CEU6 ?
- Mark as New
- Bookmark
- Subscribe
- Mute
- Subscribe to RSS Feed
- Permalink
- Email to a Friend
- Report Inappropriate Content
‎2024-12-31 4:58 AM - edited ‎2024-12-31 4:58 AM
Please avoid ALL CAPS
If you want to copy existing EVAL, NUCLEO, DISCO designs you can find schematics and BoM under the "CAD Resources" tabs on the product pages.
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
‎2024-12-31 5:14 AM
- Mark as New
- Bookmark
- Subscribe
- Mute
- Subscribe to RSS Feed
- Permalink
- Email to a Friend
- Report Inappropriate Content
‎2024-12-31 5:44 PM
You have the option to use a real XTAL (crystal) or a CMOS OSC digital source.
The difference is just:
- a XTAL (crystal) needs a configuration on CLK _Config as XTAL (both pins used, in analog OSC mode)
- a CMOS OSC source needs a configuration in "bypass mode" (just one pin used, as digital OSC signal)
As long as the XTAL (or CMOS OSC) frequency is within the valid range (check datasheet) - all fine and the CLK system config can be adjusted to your external CLK source.
Just check what is the min and max external frequency.
Best is:
check similar schematics for your MCU (for similar boards). You should see how to connect a XTAL (the tiny caps needed there, a digital CMOS OSC might be easier).
If you want to connect a CMOS OSC instead: it uses just one pin and the clock source has to be set to "bypass mode" (using just one pin CLK digital input signal).
- Mark as New
- Bookmark
- Subscribe
- Mute
- Subscribe to RSS Feed
- Permalink
- Email to a Friend
- Report Inappropriate Content
‎2024-12-31 9:38 PM
selection of 8mhz crystal for sm32l462ceu6
as per datasheet C stray 10pf , and they have given this on page no 122 "For CL1 and CL2, it is recommended to use high-quality external ceramic capacitors in the 5 pF to 20 pF range (typ.)"
so we have assume load capacitance value 12.5pf , we got Cl1=Cl2= 5pf.
also ECS internation suggest "High Drive - The other extreme is more drive than the crystal and the oscillator loop can withstand. Some of the STM32 MCU’s have a HIGH DRIVE configurable setting, for these its recommended to use 12.5pF CL crystal."
so 8 mhz crystal with load capacitance value 12.5pf is right or wrong?
in reference board NUCLEO-L476RG there is 16pf load capacitance value 8mhz crystal used , which one is right?
- Mark as New
- Bookmark
- Subscribe
- Mute
- Subscribe to RSS Feed
- Permalink
- Email to a Friend
- Report Inappropriate Content
‎2025-01-01 4:13 AM
Writing in all capital letter is often understood as screaming at the readers. Consider communication in a normal voice...