cancel
Showing results for 
Search instead for 
Did you mean: 

Could use some help (just starting out)

Mark Nordstrand
Associate
Posted on May 30, 2017 at 20:54

So, a stm32 Nucleo (little sticker indicates -F411RE) was left on my desk.  I looked at tools and got System Workbench installed.  I figured a first test (of myself, the board, and the tools) would be to modify LED blink program already on the board.  The only source I've been able to find is V1.2.1 extracted from en.stsw-stm32143.zip.  

As I go through en.DM00105928.pdf (step 4.1.4 pg 18), It would seem some things are missing.  Shouldn't  there be SW4STM32 directories somewhere in the source tree?  Is this even the correct source to use?  

This discussion is locked. Please start a new topic to ask your question.
4 REPLIES 4
Khouloud GARSI
ST Employee
Posted on May 30, 2017 at 23:33

Hi

nordstrand.mark

,

Welcome to ou STM32 MCUs community

The provided examples under the 'STM32_Nucleo_FW_V1.2.1' package are not available using the SW4STM32 IDE.

I advise you to download the

https://my.st.com/content/my_st_com/en/products/embedded-software/mcus-embedded-software/stm32-embedded-software/stm32cube-embedded-software/stm32cubef4.license=14961773786html

package.

Many examples using the SW4STM32 IDE are found under the path below:

STM32Cube_FW_F4_V1.0\Projects\STM32F411RE-Nucleo\Examples\.\.\SW4STM32

Khouloud.

Andrei Chichak
Lead II
Posted on May 30, 2017 at 23:53

Ah someone did a seagull delivery (poop and run).

I did a series of blog posts about getting started with the STM32 Discovery boards (like the Nucleo's but more complex), using the SW4STM32 tool chain.

You can find all of this on embedded.fm/blog.  The index link is here: 

http://embedded.fm/blog/embedded-wednesdays

 

You should find this helpful.

Andrei from The Great White North

Posted on May 31, 2017 at 17:02

Thank you, that was what I was looking for.

Posted on June 01, 2017 at 10:44

Hi

Nordstrand.Mark

,

Happy that you have found what you're looking for

https://community.st.com/0D50X00009bMM5DSAW

Khouloud.