Could not read the Interrupt Priority after vTaskStartScheduler()
Options
- Mark as New
- Bookmark
- Subscribe
- Mute
- Subscribe to RSS Feed
- Permalink
- Email to a Friend
- Report Inappropriate Content
2018-12-12 6:24 AM
Hi All,
I want to use NVIC_GetPriority(DMA1_Channel4_IRQn) function with FreeRtos. I can use this function before the vTaskStartScheduler(); but, when I call NVIC_GetPriority(DMA1_Channel4_IRQn) function after vTaskStartScheduler();, it does not work do you have any suggestion?
#include <FreeRTOS.h>
#include <queue.h>
#include <task.h>
/* -- */
static void vTest_NVIC( void *pvParameters )
{
tprintf("\r\nTask Started...");
/* -- */
while(1) {
/* -- */
taskENTER_CRITICAL();
tprintf("\r\npriority= %d",NVIC_GetPriority(DMA1_Channel4_IRQn));
taskEXIT_CRITICAL();
vTaskDelay(3000);;
}
}
int main()
{
portBASE_TYPE xReturn;
/* -- */
xReturn = xTaskCreate ( vTest_NVIC, ( const signed portCHAR * const )"Test_NVIC", configMINIMAL_STACK_SIZE<<4, NULL, tskIDLE_PRIORITY, NULL );
if( xReturn != pdPASS ) {
tprintf("\n\rTest_NVIC initilisation problem.\n\r");
}
NVIC_InitTypeDef NVIC_InitStructure;
NVIC_SetPriorityGrouping(3);
/* DMA1 Channel4 interrupt setting */
NVIC_InitStructure.NVIC_IRQChannel = DMA1_Channel4_IRQn;
NVIC_InitStructure.NVIC_IRQChannelPreemptionPriority = 11;
NVIC_InitStructure.NVIC_IRQChannelSubPriority = 0;
NVIC_InitStructure.NVIC_IRQChannelCmd = ENABLE;
NVIC_Init(&NVIC_InitStructure);
tprintf("\r\npriority= %d",NVIC_GetPriority(DMA1_Channel4_IRQn));
/* Now all the tasks have been started - start the scheduler. */
vTaskStartScheduler();
The output of the program is like that.
priority= 11
Task Started...
Do you have any suggestions? thanks from now
Labels:
- Labels:
-
Interrupt
This discussion is locked. Please start a new topic to ask your question.
0 REPLIES 0