Connection to FPGA with FSMC
- Mark as New
- Bookmark
- Subscribe
- Mute
- Subscribe to RSS Feed
- Permalink
- Email to a Friend
- Report Inappropriate Content
2016-05-24 7:57 AM
Hello.
I’m trying to connect a F207ZG to the Avalon-Bus of an Altera FPGA. I want to use the FSMC of the STM32. Because the STM32 and the FPGA have different clock domains, I configured the FSMC as asynchronous SRAM:
/* FSMC initialization function */
void MX_FSMC_Init(void) { FSMC_NORSRAM_TimingTypeDef Timing;/** Perform the SRAM1 memory initialization sequence
*/ hsram1.Instance = FSMC_NORSRAM_DEVICE; hsram1.Extended = FSMC_NORSRAM_EXTENDED_DEVICE; /* hsram1.Init */ hsram1.Init.NSBank = FSMC_NORSRAM_BANK1; hsram1.Init.DataAddressMux = FSMC_DATA_ADDRESS_MUX_DISABLE; hsram1.Init.MemoryType = FSMC_MEMORY_TYPE_SRAM; hsram1.Init.MemoryDataWidth = FSMC_NORSRAM_MEM_BUS_WIDTH_16; hsram1.Init.BurstAccessMode = FSMC_BURST_ACCESS_MODE_DISABLE; hsram1.Init.WaitSignalPolarity = FSMC_WAIT_SIGNAL_POLARITY_LOW; hsram1.Init.WrapMode = FSMC_WRAP_MODE_DISABLE; hsram1.Init.WaitSignalActive = FSMC_WAIT_TIMING_BEFORE_WS; hsram1.Init.WriteOperation = FSMC_WRITE_OPERATION_ENABLE; hsram1.Init.WaitSignal = FSMC_WAIT_SIGNAL_DISABLE; hsram1.Init.ExtendedMode = FSMC_EXTENDED_MODE_DISABLE; hsram1.Init.AsynchronousWait = FSMC_ASYNCHRONOUS_WAIT_ENABLE; hsram1.Init.WriteBurst = FSMC_WRITE_BURST_DISABLE; /* Timing */ Timing.AddressSetupTime = 1; Timing.AddressHoldTime = 15; Timing.DataSetupTime = 1; Timing.BusTurnAroundDuration = 1; Timing.CLKDivision = 16; Timing.DataLatency = 17; Timing.AccessMode = FSMC_ACCESS_MODE_A; /* ExtTiming */HAL_SRAM_Init(&hsram1, &Timing, NULL);
}
I designed an interface FSMC / Avalon in the FPGA. Therefore I want to use the asynchronous wait of FSMC.
But the FSMC_NWAIT signal doesn’t affect the timing of the FSMC.Does the FSMC_NWAIT signal work in asynchronous mode?
Guenter- Mark as New
- Bookmark
- Subscribe
- Mute
- Subscribe to RSS Feed
- Permalink
- Email to a Friend
- Report Inappropriate Content
2016-05-25 1:23 AM
Post relevant FSMC and GPIO register content.
JW- Mark as New
- Bookmark
- Subscribe
- Mute
- Subscribe to RSS Feed
- Permalink
- Email to a Friend
- Report Inappropriate Content
2016-05-25 8:27 AM
Hello Jan,
here the configuration of the GPIO:void MX_GPIO_Init(void)
{GPIO_InitTypeDef GPIO_InitStruct;
/* GPIO Ports Clock Enable */
__HAL_RCC_GPIOC_CLK_ENABLE(); __HAL_RCC_GPIOF_CLK_ENABLE(); __HAL_RCC_GPIOH_CLK_ENABLE(); __HAL_RCC_GPIOA_CLK_ENABLE(); __HAL_RCC_GPIOG_CLK_ENABLE(); __HAL_RCC_GPIOE_CLK_ENABLE(); __HAL_RCC_GPIOB_CLK_ENABLE(); __HAL_RCC_GPIOD_CLK_ENABLE();/*Configure GPIO pin : User_Blue_Button_Pin */
// pin 13, port c GPIO_InitStruct.Pin = User_Blue_Button_Pin; GPIO_InitStruct.Mode = GPIO_MODE_INPUT; GPIO_InitStruct.Pull = GPIO_NOPULL; HAL_GPIO_Init(User_Blue_Button_GPIO_Port, &GPIO_InitStruct);/*Configure GPIO pins : RMII_MDC_Pin RMII_RXD0_Pin RMII_RXD1_Pin */
// pin 4 and 5, port c GPIO_InitStruct.Pin = RMII_MDC_Pin|RMII_RXD0_Pin|RMII_RXD1_Pin; GPIO_InitStruct.Mode = GPIO_MODE_AF_PP; GPIO_InitStruct.Pull = GPIO_NOPULL; GPIO_InitStruct.Speed = GPIO_SPEED_FREQ_VERY_HIGH; GPIO_InitStruct.Alternate = GPIO_AF11_ETH; HAL_GPIO_Init(GPIOC, &GPIO_InitStruct);/*Configure GPIO pins : RMII_REF_CK_Pin RMII_MDIO_Pin RMII_CRS_DV_Pin */
// pin 1, 2 and 7 port a; GPIO_InitStruct.Pin = RMII_REF_CK_Pin|RMII_MDIO_Pin|RMII_CRS_DV_Pin; GPIO_InitStruct.Mode = GPIO_MODE_AF_PP; GPIO_InitStruct.Pull = GPIO_NOPULL; GPIO_InitStruct.Speed = GPIO_SPEED_FREQ_VERY_HIGH; GPIO_InitStruct.Alternate = GPIO_AF11_ETH; HAL_GPIO_Init(GPIOA, &GPIO_InitStruct);/*Configure GPIO pin : RMII_TXD1_Pin */
// pin 13, port b GPIO_InitStruct.Pin = RMII_TXD1_Pin; GPIO_InitStruct.Mode = GPIO_MODE_AF_PP; GPIO_InitStruct.Pull = GPIO_NOPULL; GPIO_InitStruct.Speed = GPIO_SPEED_FREQ_VERY_HIGH; GPIO_InitStruct.Alternate = GPIO_AF11_ETH; HAL_GPIO_Init(RMII_TXD1_GPIO_Port, &GPIO_InitStruct);/*Configure GPIO pins : LD3_Pin PB7 */
// pin 14, port b GPIO_InitStruct.Pin = LD3_Pin|GPIO_PIN_7; GPIO_InitStruct.Mode = GPIO_MODE_OUTPUT_PP; GPIO_InitStruct.Pull = GPIO_NOPULL; GPIO_InitStruct.Speed = GPIO_SPEED_FREQ_LOW; HAL_GPIO_Init(GPIOB, &GPIO_InitStruct);/*Configure GPIO pin : USB_PowerSwitchOn_Pin */
// pin 6, port g GPIO_InitStruct.Pin = USB_PowerSwitchOn_Pin; GPIO_InitStruct.Mode = GPIO_MODE_OUTPUT_PP; GPIO_InitStruct.Pull = GPIO_NOPULL; GPIO_InitStruct.Speed = GPIO_SPEED_FREQ_LOW; HAL_GPIO_Init(USB_PowerSwitchOn_GPIO_Port, &GPIO_InitStruct);/*Configure GPIO pin : USB_OverCurrent_Pin */
// pin 6, port g GPIO_InitStruct.Pin = USB_OverCurrent_Pin; GPIO_InitStruct.Mode = GPIO_MODE_INPUT; GPIO_InitStruct.Pull = GPIO_NOPULL; HAL_GPIO_Init(USB_OverCurrent_GPIO_Port, &GPIO_InitStruct);/*Configure GPIO pin : PC9 */
// pin 9, port c GPIO_InitStruct.Pin = GPIO_PIN_9; GPIO_InitStruct.Mode = GPIO_MODE_AF_PP; GPIO_InitStruct.Pull = GPIO_NOPULL; GPIO_InitStruct.Speed = GPIO_SPEED_FREQ_LOW; GPIO_InitStruct.Alternate = GPIO_AF0_MCO; HAL_GPIO_Init(GPIOC, &GPIO_InitStruct);/*Configure GPIO pins : USB_SOF_Pin USB_ID_Pin USB_DM_Pin USB_DP_Pin */
// pin 8, 10, 11 and 12 port a GPIO_InitStruct.Pin = USB_SOF_Pin|USB_ID_Pin|USB_DM_Pin|USB_DP_Pin; GPIO_InitStruct.Mode = GPIO_MODE_AF_PP; GPIO_InitStruct.Pull = GPIO_NOPULL; GPIO_InitStruct.Speed = GPIO_SPEED_FREQ_VERY_HIGH; GPIO_InitStruct.Alternate = GPIO_AF10_OTG_FS; HAL_GPIO_Init(GPIOA, &GPIO_InitStruct);/*Configure GPIO pin : USB_VBUS_Pin */
// pin 9, port a GPIO_InitStruct.Pin = USB_VBUS_Pin; GPIO_InitStruct.Mode = GPIO_MODE_INPUT; GPIO_InitStruct.Pull = GPIO_NOPULL; HAL_GPIO_Init(USB_VBUS_GPIO_Port, &GPIO_InitStruct);/*Configure GPIO pins : RMII_TX_EN_Pin RMII_TXD0_Pin */
// pin 11 und 13, port g GPIO_InitStruct.Pin = RMII_TX_EN_Pin|RMII_TXD0_Pin; GPIO_InitStruct.Mode = GPIO_MODE_AF_PP; GPIO_InitStruct.Pull = GPIO_NOPULL; GPIO_InitStruct.Speed = GPIO_SPEED_FREQ_VERY_HIGH; GPIO_InitStruct.Alternate = GPIO_AF11_ETH; HAL_GPIO_Init(GPIOG, &GPIO_InitStruct);/*Configure GPIO pin Output Level */
HAL_GPIO_WritePin(GPIOB, LD3_Pin|GPIO_PIN_7, GPIO_PIN_RESET);/*Configure GPIO pin Output Level */
HAL_GPIO_WritePin(USB_PowerSwitchOn_GPIO_Port, USB_PowerSwitchOn_Pin, GPIO_PIN_RESET);}
Wich additional information to configuration of FSMC do you need? Thank you. Guenter- Mark as New
- Bookmark
- Subscribe
- Mute
- Subscribe to RSS Feed
- Permalink
- Email to a Friend
- Report Inappropriate Content
2016-05-25 9:18 AM
Hi guenni,
I recommend you that you get in touch with the FSMC examples in wich examplain how to well configure the FSMC controller to access an Synchronous RAM memory. Examples at this path : STM32Cube_FW_F2_V1.3.0\Projects\STM322xG_EVAL\Examples\FSMC\FSMC_SRAM_DataMemory Have a look to this to ensure that you don't have the same issue -Hannibal-- Mark as New
- Bookmark
- Subscribe
- Mute
- Subscribe to RSS Feed
- Permalink
- Email to a Friend
- Report Inappropriate Content
2016-05-25 10:02 AM
Guenter,
I mean, read out the content of the relevant FSMC and GPIO registers after they have been initialized. Then confront them to the RM. JW- Mark as New
- Bookmark
- Subscribe
- Mute
- Subscribe to RSS Feed
- Permalink
- Email to a Friend
- Report Inappropriate Content
2016-05-30 6:09 AM
Hello,
I found some information in reference manual RM0090. The asynchronous wait, will be detected 4 HCLK before the end of memory transaction. I’ve configured AddressSetupTime = 1 and DataSetupTime = 1. Then the asynchronous wait doesn’t work. AddressSetupTime must be at least 5. Thank you for your efforts. Guenter