2012-06-22 11:54 AM
Hi,
I am using the STM32F103ZG device and looking through the reference manual (RM0008) I cannot find how, when a pin is configured as ''Input Pull-up/pull-down'', to select the pull-up or pull-down option. Having done some experimentation it appears that this can be done by setting the ports output level high (for pull-up) and low (for pull-down) operation after the pin has been configured as an input. Is this the indended way to do this? If not, an explanation on how it should be done would be appreciated. Regards Farmer #gpio-mode2012-06-22 1:24 PM
In RM0008 it is described in Table 20. Port bit configuration table, Page 156
2012-06-22 3:37 PM
Looked at the very table, must have just missed it. Problem sorted - many thanks.
Regards FarmerWe’re moving the ST Community to a new platform to give you a better and more reliable community experience.