2012-06-21 12:40 AM
Hello.
I have a probem with the ISO IN Endpoint. Double buffering is not working.The STM32F103RD is sending right data only from one buffer. Data from another buffer is wrong.My code: /* Initialize Endpoint 1 */ SetEPType(ENDP1, EP_ISOCHRONOUS); SetEPDblBuffAddr(ENDP1, ENDP1_BUF0Addr, ENDP1_BUF1Addr); ClearDTOG_RX(ENDP1); ClearDTOG_TX(ENDP1); ToggleDTOG_RX(ENDP1); SetEPTxStatus(ENDP1, EP_TX_NAK); SetEPRxStatus(ENDP1, EP_RX_DIS);void SOF_Callback(void){ if(bDeviceState == CONFIGURED) { if (GetENDPOINT(ENDP1) & EP_DTOG_RX) { /*write to ENDP1_BUF0Addr buffer*/ UserToPMABufferCopy(USB_Buf, ENDP1_BUF0Addr, USB_Idx); SetEPDblBuf0Count(ENDP1,EP_DBUF_IN ,USB_Idx); } else { /*write to ENDP1_BUF1Addr buffer*/ UserToPMABufferCopy(USB_Buf, ENDP1_BUF1Addr, USB_Idx); SetEPDblBuf1Count(ENDP1,EP_DBUF_IN ,USB_Idx); } SetEPTxValid(ENDP1); }}Is anyone know what is a problem?2012-06-22 12:23 PM
At initialization,
SetEPTxStatus(ENDP1, EP_TX_NAK); <--- SetEPTxStatus(ENDP1, EP_TX_VALID); NAK is not allowed on isoc endpoint. Just VALID or DISable. In SOF_Callback(void), SetEPTxValid(ENDP1); <--- FreeUserBuffer(ENDP1, EP_DBUF_IN); TX status doesn't change after transmission. It stays in VALID. So, doesn't need to make it VALID. FreeUserBuffer() toggles DTOG_RX TsuneoWe’re moving the ST Community to a new platform to give you a better and more reliable community experience.