2010-03-12 01:33 AM
configure a general purpose TIMx (x=2,3,4) same as Systick on STM32F103B
2011-05-17 04:43 AM
#define CPUCLOCK (36.0) // CPU Clock MHz
{ int i; for(i=0; i<10; i++) { u32 a, b; do { a = SystemTick; // 1ms counter off SYSTICK interrupt b = SystemTick; } while(a == b); // Sychronize on SYSTICK STOPWATCH_START Sleep(10); // 10ms delay STOPWATCH_STOP printf(''%10d cycles, %7.4lf ms\n'',cyc[1],((1.0 / (CPUCLOCK * 1000.0)) * (double)cyc[1])); // 36 MHz clock, milliseconds from cycles } } 360091 cycles, 10.0025 ms 360091 cycles, 10.0025 ms 360089 cycles, 10.0025 ms 360089 cycles, 10.0025 ms 360089 cycles, 10.0025 ms 360091 cycles, 10.0025 ms 360175 cycles, 10.0049 ms 360089 cycles, 10.0025 ms 360177 cycles, 10.0049 ms 360177 cycles, 10.0049 ms2011-05-17 04:43 AM
>>with the method you suggested, we should using J-TRACE isn't it ? I have only J-LINK;
The cycle counting works with the trace hardware inside the STM32 core, it *does not* require a J-TRACE or J-LINK. It works with stock STM32F103 devices, and probably the rest of the family. If the delay routine is using the SYSTICK at 1 ms, then the 10 ms delay could be between 9-11 ms depending on when you catch the counter. You could always get additional accuracy by using SysTick->VAL which counts down at 1/8000 of a millisecond (assuming 64 MHz, and a /8 prescale, and a 1 ms interrupt) -Clive2011-05-17 04:43 AM
Using Timer 4, less resolution/precision, 16-bit register
{ TIM_TimeBaseInitTypeDef TIM_TimeBaseStructure; RCC_APB1PeriphClockCmd(RCC_APB1Periph_TIM4, ENABLE); TIM_DeInit(TIM4); TIM_TimeBaseStructure.TIM_Period = 0xffff; TIM_TimeBaseStructure.TIM_Prescaler = 15; TIM_TimeBaseStructure.TIM_ClockDivision = 0x0; TIM_TimeBaseStructure.TIM_CounterMode = TIM_CounterMode_Up; TIM_TimeBaseInit(TIM4, &TIM_TimeBaseStructure ); //TIM_ARRPreloadConfig(TIM4, ENABLE); TIM4->EGR |= 0x01; } { u16 tim[2]; int i; for(i=0; i<10; i++) { u32 a, b; a = SystemTick; do { b = SystemTick; } while(a == b); tim[0] = TIM4->CNT; TIM4->CR1 |= 1; Sleep(10); TIM4->CR1 &= ~1; tim[1] = TIM4->CNT; tim[1] = tim[1] - tim[0]; printf(''%10d cycles, %7.4lf ms\n'',tim[1],((16.0 / (CPUCLOCK * 1000.0)) * (double)tim[1])); } putchar('\n'); } 22510 cycles, 10.0044 ms 22510 cycles, 10.0044 ms 22511 cycles, 10.0049 ms 22511 cycles, 10.0049 ms 22510 cycles, 10.0044 ms 22511 cycles, 10.0049 ms 22510 cycles, 10.0044 ms 22510 cycles, 10.0044 ms 22511 cycles, 10.0049 ms 22510 cycles, 10.0044 ms2011-05-17 04:43 AM
One more argument FOR SysTick:
reading TIMx through APB brings jitter and delay in range (1+ratio) AHB cycles due to resynchronization between APB and AHB in the bridge. Reading systick is done on internal Cortex bus => very low latency, cycle precise. Btw. even if any jitter might be induced, the whole MCU would be delayed with the same amount of time => it's still cycle precise 🙂2011-05-17 04:43 AM
Hi Edison,
Would you explain this with more details please?
Slim