cancel
Showing results for 
Search instead for 
Did you mean: 

Complementary output PWM low can not sink current

ZDu
Associate

​I used TIM1 to generate complementary output PWM signals. The EGR register is used to generate a COMG event to update the output signals. The output waveforms are good. But I found the output can't absorb sink current when it is low, a 2k pull up resistor will cause low voltage higher than 3V. Any one has any clues? Thanks. 

This discussion is locked. Please start a new topic to ask your question.
0 REPLIES 0