cancel
Showing results for 
Search instead for 
Did you mean: 

Coherent dual channel (multimode) sampling on STM32F4

darek
Associate
Posted on June 12, 2015 at 12:02

Hi All,

  I am learning how the  ADCs  modes are working on the ST32F4 MCU (using Olimex board). I got operational  ADCs (running independently)  in 

 a single a and continuous mode.

The next step is to get a coherent sampling from two ADCs (for all cases I am explicitly polling measurements within my program). 

The multimode configuration is presented below.  I would like to read the data from both (ADC1 and ADC2) converters into an 

array of samples using  the following function (S1, S2 are for  debugging purposes only):

void Get_RawSamples( __IO uint16_t  Ch1[],  __IO uint16_t  Ch2[], int NumSamples)

{

    int16_t i, S1,S2 ;

    __IO uint32_t S12;

  for (i  =  0;  i  <  NumSamples;  i++)

  {

      ADC_SoftwareStartConv(ADC1);

      while(ADC_GetFlagStatus(ADC1, ADC_FLAG_EOC) == RESET);

       S1 =  ADC_GetConversionValue(ADC1);

       Ch1[i] = S1;

       S2  = ADC_GetConversionValue(ADC2);

       Ch2[i] =  S2;

  }

} /* end Get_RawSamples */

According to the documentation, to retrieve  samples from multiple ADCs I should  use the 

 ADC_GetMultiModeConversionValue() function. 

When I call  the ADC_GetConvertionValue  function for each ADC, I am getting correct values (connected a 1.5 V battery, and checked 

against the digital multimeter measurements).  

When I replace the content of the loop with:

     

      ADC_SoftwareStartConv(ADC1); //this is the master 

      while(ADC_GetFlagStatus(ADC1, ADC_FLAG_EOC) == RESET);

      S12 =  ADC_GetMultiModeConversionValue();

 

and run/debug it, the  value of S12 is always zero. 

So, I have some questions:

  1. If I call ADC_GetConversionValue for each ADC  separately do I get coherent measurements ? 

  2. Why the value of S12 is zero? Is there any special way of dealing with  the multimode data conversion?

  

  After getting the ADCs in the  polling mode working, I will switch to the DMA approach  with timers to control sampling rate.

  Thanks in advance for your help.

 Cheers,

   Darek 

P.S. I have noticed that calling:

     ADC_EOCOnEachRegularChannelCmd(ADC1, ENABLE) 

     (or ADC_EOCOnEachRegularChannelCmd(ADC1, DISABLE)  for tests)

 in  the configuration  of the ADCs does not have any influence on the behaviour of my code.

/* ADC Configuration */

void Configure_ADCs(void)

{

    ADC_InitTypeDef       ADC_InitStructure;

    ADC_CommonInitTypeDef ADC_CommonInitStructure;

   ADC_CommonInitStructure.ADC_Mode = ADC_DualMode_RegSimult; 

   ADC_CommonInitStructure.ADC_TwoSamplingDelay = 0;

   ADC_CommonInitStructure.ADC_DMAAccessMode = ADC_DMAAccessMode_Disabled;

   ADC_CommonInitStructure.ADC_Prescaler = ADC_Prescaler_Div2;

   ADC_CommonInit(&ADC_CommonInitStructure);

   ADC_InitStructure.ADC_Resolution = ADC_Resolution_12b;

   ADC_InitStructure.ADC_ContinuousConvMode = DISABLE;

   ADC_InitStructure.ADC_ScanConvMode = DISABLE;

   ADC_InitStructure.ADC_ExternalTrigConvEdge = ADC_ExternalTrigConvEdge_None;

   ADC_InitStructure.ADC_ExternalTrigConv = ADC_ExternalTrigConv_T2_TRGO; 

   ADC_InitStructure.ADC_DataAlign = ADC_DataAlign_Right;

   ADC_InitStructure.ADC_NbrOfConversion = 1;

   ADC_Init(ADC1,&ADC_InitStructure);

   ADC_Init(ADC2,&ADC_InitStructure);

   ADC_RegularChannelConfig(ADC1, ADC_Channel_5,1, ADC_SampleTime_3Cycles);

   ADC_RegularChannelConfig(ADC2, ADC_Channel_6,1, ADC_SampleTime_3Cycles);

   ADC_Cmd(ADC1,ENABLE);

   ADC_Cmd(ADC2,ENABLE);

  ADC_EOCOnEachRegularChannelCmd(ADC1, ENABLE);

} /* end Configure_ADCs */

This discussion is locked. Please start a new topic to ask your question.
2 REPLIES 2
Posted on June 12, 2015 at 15:15

I'd go directly for the DMA+TIM implementation, as that's how you'd actually want to pace sampling.

[DEAD LINK /public/STe2ecommunities/mcu/Lists/cortex_mx_stm32/Flat.aspx?RootFolder=/public/STe2ecommunities/mcu/Lists/cortex_mx_stm32/stm32f207%20ADC%2BTIMER%2BDMA%20%20Poor%20Peripheral%20Library%20Examples&FolderCTID=0x01200200770978C69A1141439FE559EB459D7580009C4E14902C3CDE46A77F0FFD06506F5B&currentviews=4333]https://my.st.com/public/STe2ecommunities/mcu/Lists/cortex_mx_stm32/Flat.aspx?RootFolder=%2Fpublic%2FSTe2ecommunities%2Fmcu%2FLists%2Fcortex_mx_stm32%2Fstm32f207%20ADC%2BTIMER%2BDMA%20%20Poor%20Peripheral%20Library%20Examples&FolderCTID=0x01200200770978C69A1141439FE559EB459D7580009C4E14902C3CDE46A77F0FFD06506F5B¤tviews=4333

Perhaps you can work this backward to manually polling the EOC

Tips, Buy me a coffee, or three.. PayPal Venmo
Up vote any posts that you find helpful, it shows what's working..
darek
Associate
Posted on June 14, 2015 at 08:33

Hi Clive1,

  thanks for the link.  I will go for that solution in the future.  Just curious,  did anybody get the multimode (at least dual) ADCs working in the polling mode?

  If yes, what is the right way of doing the data extraction?

Cheers,

   Darek