2012-03-23 8:32 PM
Dear All:
I try to pass my CMOS data to ethernet interface through DMA. (Before transfer to ethernet interface, I will add bmp file header.)I already show the CMOS data on my LCD. But I don't have any idea how to pass data to ethernet interface.I have readed the sample code, LwIP, which in stander library director.My plan is add my CMOS control code in LwIP (httpserver-standalone project).Anyone has experience or idea about this? Would you please give me some idea to do this?Thanks.2012-04-27 6:07 AM
Hi, Friends:
Can you please give some advice or practice?
Now I'm not the slightest clue how to proceed.
How do I let the platform to reply my java script request?I think my problem may be a bit stupid, but I really want to finish it.
So, please. If you have any idea or any suggestion for me, please told me.Thanks Simon2012-04-28 3:05 AM
Dear all:
Does anyone using FSMC to control TFT and Ex-SRAM together?I using CMOS to catch the image and DMA2_Stream1 to move data to Ex-SRAM.My question isFSMC time settings I need to separate the settings? Or should be based on which one to set? TFT or Ex_SRAM?
Because I found image show on TFT is good but on web side (read from Ex-SRAM) has color error.Simon2012-04-28 9:15 AM
Because I found image show on TFT is good but on web side (read from Ex-SRAM) has color error.
This is more likely because the BMP encoding is not identical to the TFT one. You need to understand the various encoding schemes, and how to translate between them. You could always post the BMP, and you could also post the video/graphic format the camera uses, or a link to it's documentation. These are things which would permit others to provide more useful analysis. As I've suggested previously there are some simple ways of confirming that the data on the STM32 side matches that on the PC side.2012-04-30 1:50 AM
Dear Clive1:
Thanks for you remind me to check the data format.I found the bug of my image data.I forgot add the color mask, that what my image always color error.Thank you again.Now I am try to fix another problem. How to load image on the web which don't useweb refresh.Simon2012-05-14 12:13 AM
Dear all:
I am back. I already fixed color error and don't refresh whole page to show image.Thanks guys, thanks your kindly help.Now, I have a question about DMA doublebuffer mode.Double buffer mode:M0AR -> Buffer 0 start addressM1AR -> Buffer 1 start addressDoes it means filled two buffer at one time? Because I can't found any data store from M1AR . I can not found any detail description about double buffer mode in RF document.Please if you have any experience using DCMI and DMA bouble buffer mode please to share I willing to read!
Thanks Simon