cancel
Showing results for 
Search instead for 
Did you mean: 

migration from uPSD3200 to STM32

rs11
Associate II
Posted on November 18, 2008 at 20:08

migration from uPSD3200 to STM32

This discussion is locked. Please start a new topic to ask your question.
4 REPLIES 4
rs11
Associate II
Posted on May 17, 2011 at 12:50

Is there any benchmark data that compares the code size and data size of an existing software which migrates from uPSD3200(8032 based) to STM32 (Cortex-M3 based)?

I would imagine that the 8-bit,CISC in 8032 to 16/32-bit,RISC in Cortex-M3 should cause the code size to increase (dont know by what % though!). Can someone throw some light here..

I am hopeful that the data size would remain the same since Cortex-M3 boasts of having un-aligned data access built into the hardware, letting the compilers pack all the data in memory. Can someone tell me which compilers does (or does not)take this into account?

obtronix
Associate II
Posted on May 17, 2011 at 12:50

Cortex code size is about 1/4 the size of 8051 code according to

www.iqmagazineonline.com/IQ/IQ16/LowRes.pdfs/Luminary(pg28-32)IQ16.pdf

st3
Associate II
Posted on May 17, 2011 at 12:50

Quote:

On 04-11-2008 at 04:55, Anonymous wrote:

Cortex code size is about 1/4 the size of 8051 code according to

http://www.iqmagazineonline.com/IQ/IQ16/LowRes.pdfs/Luminary(pg28-32)IQ16.pdf

All that article actually says is,

Quote:

... ARM reports that Cortex-M3 requires about 1/4th the code space of an 8051.

No reference is given to how ARM arrived at that figure, how generally applicable it is, etc, etc - and, of course, ARM's is hardly an independent view in this matter, is it...?! ;)

The context in the article is,

Quote:

... an 8-bit CISC machine like the 8051 is actually a very inefficient architecture for modern high-level software.

Which is assuming that the 8051 is being used inappropriately - so, if you have a well-optimised, appropriate 8051 application, I guess the comparison will be very different...?

So, does anyone have a reference to the original ARM publication that made this ''25%'' claim?

[ This message was edited by: st7 on 11-11-2008 18:12 ]

[ This message was edited by: st7 on 11-11-2008 18:13 ]

st3
Associate II
Posted on May 17, 2011 at 12:50

Quote:

if you have a well-optimised, appropriate 8051 application, I guess the comparison will be very different...?

The Keil documentation seems to provide a more realistic illustration:

http://www.keil.com/support/man/docs/gs/gs_ma_portaccess.htm

illustrates a case where the 8051 requires only 25% of the code size of a corresponding Cortex program;

Whereas

http://www.keil.com/support/man/docs/gs/gs_ma_pointeraccess.htm

illustrates a case where the Cortes requires 25% of the code size of a corresponding 8051 program!

Thus, as I suspected, it depends very much on the specific nature of your particular application - and any so-called ''general'' figures you may see must be taken with great caustion!