cancel
Showing results for 
Search instead for 
Did you mean: 

CDC Standalone STM3210E_EVAL change uart

vbruno1
Associate III
Posted on April 29, 2016 at 17:30

I would change uart in CDC standalone example for STM3210E_EVAL by uart1 to uart2.

I changed the code in this mode:

/* Definition for USARTx clock resources */
#define USARTx USART2
#define USARTx_CLK_ENABLE() __HAL_RCC_USART2_CLK_ENABLE();
#define DMAx_CLK_ENABLE() __HAL_RCC_DMA1_CLK_ENABLE()
#define USARTx_RX_GPIO_CLK_ENABLE() __HAL_RCC_GPIOA_CLK_ENABLE()
#define USARTx_TX_GPIO_CLK_ENABLE() __HAL_RCC_GPIOA_CLK_ENABLE() 
#define USARTx_FORCE_RESET() __HAL_RCC_USART2_FORCE_RESET()
#define USARTx_RELEASE_RESET() __HAL_RCC_USART2_RELEASE_RESET()
/* Definition for USARTx Pins */
#define USARTx_TX_PIN GPIO_PIN_2
#define USARTx_TX_GPIO_PORT GPIOA 
#define USARTx_RX_PIN GPIO_PIN_3
#define USARTx_RX_GPIO_PORT GPIOA 
/* Definition for USARTx's NVIC: used for receiving data over Rx pin */
#define USARTx_IRQn USART2_IRQn
#define USARTx_IRQHandler USART2_IRQHandler
/* Definition for USARTx's DMA: used for transmitting data over Tx pin */
#define USARTx_TX_DMA_STREAM DMA1_Channel4
#define USARTx_RX_DMA_STREAM DMA1_Channel5
/* Definition for USARTx's NVIC */
#define USARTx_DMA_TX_IRQn DMA1_Channel4_IRQn
#define USARTx_DMA_RX_IRQn DMA1_Channel5_IRQn
#define USARTx_DMA_TX_IRQHandler DMA1_Channel4_IRQHandler
#define USARTx_DMA_RX_IRQHandler DMA1_Channel5_IRQHandler
/* Definition for TIMx clock resources */
#define TIMx TIM3
#define TIMx_CLK_ENABLE __HAL_RCC_TIM3_CLK_ENABLE
#define TIMx_FORCE_RESET() __HAL_RCC_USART2_FORCE_RESET()
#define TIMx_RELEASE_RESET() __HAL_RCC_USART2_RELEASE_RESET()
/* Definition for TIMx's NVIC */
#define TIMx_IRQn TIM3_IRQn
#define TIMx_IRQHandler TIM3_IRQHandler

But don't work good.I can test the code directly on the boardSTM3210E_EVAL. If I write on the form of the hyperterminal USART, on the usb form I view strings of characters. Although, when I write 2 identical characters in a row only one of them appears correttemente. As if I write from the USB form, the usart form is blank. Usb hypertermial form a lockout. Tips, plesae?
This discussion is locked. Please start a new topic to ask your question.
1 REPLY 1
Walid FTITI_O
Senior II
Posted on May 25, 2016 at 17:31

Hi bruno.vincenzo,

You should change the DMA channel relevant to USART2. (see reference manual RM0008 -> Table Summary of DMA1 requests for each channel)

#define USARTx_TX_DMA_STREAM DMA1_Channel4
#define USARTx_RX_DMA_STREAM DMA1_Channel5

should be changed by

#define USARTx_TX_DMA_STREAM DMA1_Channel7

#define USARTx_RX_DMA_STREAM DMA1_Channel6
 -Hannibal-