cancel
Showing results for 
Search instead for 
Did you mean: 

Capteur Internal Temperature sensor..!!

oussama-laribi
Associate II
Posted on April 27, 2013 at 00:26

Hi

I find problems with capateur internal temperature sensor STM32F4 Discovery, I have measured as false (-80.50...-45.00...-60.50 ).

I know if my code is wrong or the formula that calculates the temperature.

I hope there's someone there who has decided to issue ..!

I hope to find the right code or the right formula.

thank you..
4 REPLIES 4
raptorhal2
Lead
Posted on April 27, 2013 at 19:41

Check the F4 Standard Peripheral Library examples for guidance. If that doesn't work, post your code.

Cheers, Hal

oussama-laribi
Associate II
Posted on April 27, 2013 at 20:43

The original post was too long to process during our migration. Please click on the provided URL to read the original post. https://st--c.eu10.content.force.com/sfc/dist/version/download/?oid=00Db0000000YtG6&ids=0680X000006I6mp&d=%2Fa%2F0X0000000bvQ%2F0gf4DYlmjTOqdcsO4.FBltQnS2BUwM8laM1r4KiFARI&asPdf=false
raptorhal2
Lead
Posted on April 29, 2013 at 16:15

Two problems:

The minimum ADC sampling time for the temperature channel is 10 microseconds. See Section 5.3.21 in the F4 datasheet. Change the sampling to at least 110 cycles.

After

ADC_InitStructure.ADC_ExternalTrigConvEdge = ADC_ExternalTrigConvEdge_None;

Add

ADC_InitStructure.ADC_ExternalTrigConv = 0;

Cheers, Hal

oussama-laribi
Associate II
Posted on April 30, 2013 at 01:03

thank you Hal

after handling with the equation .. it's oky here is the code ..: cheers, Lary.

/* Includes ------------------------------------------------------------------*/
#include ''stm32f4_discovery.h''
#include <
stdio.h
>
#include ''main.h''
#include <
math.h
>
#define ADC1_DR_ADDRESS ((uint32_t)0x4001204C)
/*************declaration*****************/
double Voltage = 0;
__IO uint32_t ValADC = 0;
double temp = 0;
void ADC1_DMA_Config(void);
void Delay(__IO uint32_t nCount);
/*********************Configuration ADC&DMA**********************************************/
void ADC1_DMA_Config(void)
{
ADC_InitTypeDef ADC_InitStructure;
ADC_CommonInitTypeDef ADC_CommonInitStructure;
DMA_InitTypeDef DMA_InitStructure;
GPIO_InitTypeDef GPIO_InitStructure;
RCC_AHB1PeriphClockCmd(RCC_AHB1Periph_DMA2| RCC_AHB1Periph_GPIOD, ENABLE);
RCC_APB2PeriphClockCmd(RCC_APB2Periph_ADC1, ENABLE);
DMA_DeInit(DMA2_Stream0);
DMA_InitStructure.DMA_Channel = DMA_Channel_0;
DMA_InitStructure.DMA_PeripheralBaseAddr = (uint32_t)ADC1_DR_ADDRESS;
DMA_InitStructure.DMA_Memory0BaseAddr = (uint32_t)&ValADC;
DMA_InitStructure.DMA_DIR = DMA_DIR_PeripheralToMemory;
DMA_InitStructure.DMA_BufferSize = 1;
DMA_InitStructure.DMA_PeripheralInc = DMA_PeripheralInc_Disable;
DMA_InitStructure.DMA_MemoryInc = DMA_MemoryInc_Disable;
DMA_InitStructure.DMA_PeripheralDataSize = DMA_PeripheralDataSize_HalfWord;
DMA_InitStructure.DMA_MemoryDataSize = DMA_MemoryDataSize_HalfWord;
DMA_InitStructure.DMA_Mode = DMA_Mode_Circular;
DMA_InitStructure.DMA_Priority = DMA_Priority_High;
DMA_InitStructure.DMA_FIFOMode = DMA_FIFOMode_Disable;
DMA_InitStructure.DMA_FIFOThreshold = DMA_FIFOThreshold_HalfFull;
DMA_InitStructure.DMA_MemoryBurst = DMA_MemoryBurst_Single;
DMA_InitStructure.DMA_PeripheralBurst = DMA_PeripheralBurst_Single;
DMA_Init(DMA2_Stream0, &DMA_InitStructure);
DMA_Cmd(DMA2_Stream0, ENABLE);
GPIO_DeInit(GPIOD);
GPIO_InitStructure.GPIO_Pin = GPIO_Pin_12 | GPIO_Pin_13 | GPIO_Pin_14| GPIO_Pin_15;
GPIO_InitStructure.GPIO_Mode =GPIO_Mode_OUT ;
GPIO_InitStructure.GPIO_OType = GPIO_OType_PP;
GPIO_InitStructure.GPIO_Speed = GPIO_Speed_25MHz;
GPIO_InitStructure.GPIO_PuPd = GPIO_PuPd_DOWN ;
GPIO_Init(GPIOD,&GPIO_InitStructure);
ADC_CommonInitStructure.ADC_Mode = ADC_Mode_Independent;
ADC_CommonInitStructure.ADC_Prescaler = ADC_Prescaler_Div2;
ADC_CommonInitStructure.ADC_DMAAccessMode = ADC_DMAAccessMode_Disabled;
ADC_CommonInitStructure.ADC_TwoSamplingDelay = ADC_TwoSamplingDelay_5Cycles;
ADC_CommonInit(&ADC_CommonInitStructure);
ADC_InitStructure.ADC_Resolution = ADC_Resolution_12b;
ADC_InitStructure.ADC_ScanConvMode = DISABLE;
ADC_InitStructure.ADC_ContinuousConvMode = ENABLE;
ADC_InitStructure.ADC_ExternalTrigConvEdge = ADC_ExternalTrigConvEdge_None;
ADC_InitStructure.ADC_ExternalTrigConv = 0;
ADC_InitStructure.ADC_DataAlign = ADC_DataAlign_Right;
ADC_InitStructure.ADC_NbrOfConversion = 1;
ADC_Init(ADC1, &ADC_InitStructure);
ADC_DMACmd(ADC1, ENABLE);
ADC_RegularChannelConfig(ADC1, ADC_Channel_TempSensor, 1, ADC_SampleTime_480Cycles);
ADC_TempSensorVrefintCmd(ENABLE);
ADC_DMARequestAfterLastTransferCmd(ADC1, ENABLE);
ADC_Cmd(ADC1, ENABLE);
}
/****************************Programme Principal********************************************/
int main(void)
{
ADC1_DMA_Config();
ADC_SoftwareStartConv(ADC1);
Voltage = (ValADC *3300)/4095;
temp = ((Voltage - 760)/2.5)+25;
/********************************************/
void Delay(__IO uint32_t nCount)
{
while(nCount--)
{
}
}
#ifdef USE_FULL_ASSERT
void assert_failed(uint8_t* file, uint32_t line)
{
while (1)
{
}
}
#endif