Cannot change system speed for STM32F746IG
- Mark as New
- Bookmark
- Subscribe
- Mute
- Subscribe to RSS Feed
- Permalink
- Email to a Friend
- Report Inappropriate Content
‎2016-07-06 12:10 AM
I designed a PCB and I am programming the STM32F746IG via a FT2232D chip. I have the 4 x JTAG signals connected to the STM32.
I generate code with MXCube, it compiles, but when I run it, Crossworks goes into an enless loop giving me gives me ''Stopped by Vector Catch''. I have pin pointed it to the function : main.c -> SystemClock_Config(void) -> ''if (HAL_RCC_OscConfig(&RCC_OscInitStruct) != HAL_OK)'' -> ''__HAL_RCC_PLL_ENABLE();'' (just after the call to ''WRITE_REG(...)'')I also used MXCube to generate a Keil MDK V5 project, it compiled, but the same happened in the Keil development environment. If I remove the call to ''SystemClock_Config(void)'' the program works.
How do one change the clock frequency of the PLL to 216MHz?Please advise!Thanks- Mark as New
- Bookmark
- Subscribe
- Mute
- Subscribe to RSS Feed
- Permalink
- Email to a Friend
- Report Inappropriate Content
‎2016-07-06 6:27 AM
So do you have an external crystal on your design? At what frequency does it run?
The PLL settings are just a couple of simple multiplication and division computations. Review the Reference ManualUp vote any posts that you find helpful, it shows what's working..
- Mark as New
- Bookmark
- Subscribe
- Mute
- Subscribe to RSS Feed
- Permalink
- Email to a Friend
- Report Inappropriate Content
‎2016-07-09 9:19 AM
- Mark as New
- Bookmark
- Subscribe
- Mute
- Subscribe to RSS Feed
- Permalink
- Email to a Friend
- Report Inappropriate Content
‎2016-07-09 9:21 AM
- Mark as New
- Bookmark
- Subscribe
- Mute
- Subscribe to RSS Feed
- Permalink
- Email to a Friend
- Report Inappropriate Content
‎2016-07-10 6:07 AM
The forum does not support posting from mobile devices very well. You'd want to use Firefox, or post from a desktop.
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
‎2016-07-11 3:43 AM
Hi du_toit.jurie,
You should check if you have configured you system clock source HSI or HSE and if you are applying the right parameters there. If HSE is used, check that you have the rignt 25MHz crystal. I give you .ioc example file ( see attached)for a test similar to your case done using CubeMxthat can help you (HSE, 216Mhz). Otherwise, try to check the '' RCC_ClockConfig'' example in the library at this path: STM32Cube_FW_F7_V1.4.0\Projects\STM32F769I_EVAL\Examples\RCC\RCC_ClockConfig -Hannibal- ________________ Attachments : F7_RCC.ioc : https://st--c.eu10.content.force.com/sfc/dist/version/download/?oid=00Db0000000YtG6&ids=0680X000006HthG&d=%2Fa%2F0X0000000aVs%2Fo34kgFOaQxO1IpNFM7X0fUYbKdX5PCutAY_KxGHHZUg&asPdf=false