cancel
Showing results for 
Search instead for 
Did you mean: 

Can't see downlink message with I-cube-lrwan1 and B-L072Z

maxence forget
Associate II
Posted on May 18, 2017 at 09:45

Hi,

I use a Nemeus pico gateway and a B-L072Z-LRWAN1 with the I-CUBE-LRWAN software.

I displayed uplink message with a python scrypt running on a Raspberry Pi.

Nevertheless, i can't see downlink message like the join accept message.

How can i fixed this problem? I have to change something in the end node program of I-CUBE?

Thanks in advance

This discussion is locked. Please start a new topic to ask your question.
2 REPLIES 2
Amel NASRI
ST Employee
Posted on May 23, 2017 at 15:31

Hi

forget.maxence

‌,

Do you still face the reported issue?

Is it related to the one reported in

https://community.st.com/0D70X000006SsLLSA0

which is already fixed?

Please keep us informed.

-Amel

To give better visibility on the answered topics, please click on Accept as Solution on the reply which solved your issue or answered your question.

Posted on May 24, 2017 at 09:05

Hello,

The problem is not fixed. My purpose is to see frame during the join procedure or to see ACK message. Is it possible? Should i modify the code of my device or is it a gateway problem?

Thanks in advance.