can't escape while loop in SystemClock_Config();
- Mark as New
- Bookmark
- Subscribe
- Mute
- Subscribe to RSS Feed
- Permalink
- Email to a Friend
- Report Inappropriate Content
‎2018-06-14 12:35 AM
So i noticed something interesting. When setting up a project with cube or looking at a ST example for USB host the Config for system clock is like this.
RCC_OscInitTypeDef RCC_OscInitStruct;
RCC_ClkInitTypeDef RCC_ClkInitStruct;
/**Configure the main internal regulator output voltage */
__HAL_RCC_PWR_CLK_ENABLE(); __HAL_PWR_VOLTAGESCALING_CONFIG(PWR_REGULATOR_VOLTAGE_SCALE1);
/**Initializes the CPU, AHB and APB busses clocks */
RCC_OscInitStruct.OscillatorType = RCC_OSCILLATORTYPE_LSI|RCC_OSCILLATORTYPE_HSE; RCC_OscInitStruct.HSEState = RCC_HSE_ON;
RCC_OscInitStruct.LSIState = RCC_LSI_ON;
RCC_OscInitStruct.PLL.PLLState = RCC_PLL_ON;
RCC_OscInitStruct.PLL.PLLSource = RCC_PLLSOURCE_HSE;
RCC_OscInitStruct.PLL.PLLM = 25;
RCC_OscInitStruct.PLL.PLLN = 192;
RCC_OscInitStruct.PLL.PLLP = RCC_PLLP_DIV2;
RCC_OscInitStruct.PLL.PLLQ = 4;
HAL_RCC_OscConfig(&RCC_OscInitStruct);
/**Initializes the CPU, AHB and APB busses clocks */
RCC_ClkInitStruct.ClockType = RCC_CLOCKTYPE_HCLK|RCC_CLOCKTYPE_SYSCLK |RCC_CLOCKTYPE_PCLK1|RCC_CLOCKTYPE_PCLK2;
RCC_ClkInitStruct.SYSCLKSource = RCC_SYSCLKSOURCE_PLLCLK;
RCC_ClkInitStruct.AHBCLKDivider = RCC_SYSCLK_DIV1;
RCC_ClkInitStruct.APB1CLKDivider = RCC_HCLK_DIV4;
RCC_ClkInitStruct.APB2CLKDivider = RCC_HCLK_DIV2;
HAL_RCC_ClockConfig(&RCC_ClkInitStruct, FLASH_LATENCY_3);
/**Configure the Systick interrupt time */
HAL_SYSTICK_Config(HAL_RCC_GetHCLKFreq()/1000);
/**Configure the Systick */
HAL_SYSTICK_CLKSourceConfig(SYSTICK_CLKSOURCE_HCLK);
When the HAL_RCC_OscConfig(&RCC_OscInitStruct); runs there is a while and the only way to escape from it is by reading the Systemtick which is not configured yet
:(
/* Wait till HSE is ready */
while(__HAL_RCC_GET_FLAG(RCC_FLAG_HSERDY) == RESET) {
if((HAL_GetTick() - tickstart ) > HSE_TIMEOUT_VALUE)
{ return HAL_TIMEOUT; }
}
- Mark as New
- Bookmark
- Subscribe
- Mute
- Subscribe to RSS Feed
- Permalink
- Email to a Friend
- Report Inappropriate Content
‎2018-06-14 1:23 AM
I'm not going to dig into Cube/CubeMX internals: Isn't systick interrupt already enabled in the startup code, i.e. before entering main()?
JW
- Mark as New
- Bookmark
- Subscribe
- Mute
- Subscribe to RSS Feed
- Permalink
- Email to a Friend
- Report Inappropriate Content
‎2018-06-14 5:23 AM
I put a breakpoint in the interrupt it's does not enter and
systick
stays zero- Mark as New
- Bookmark
- Subscribe
- Mute
- Subscribe to RSS Feed
- Permalink
- Email to a Friend
- Report Inappropriate Content
‎2018-06-15 5:52 AM
Hello!
Systick is allready initialized before clock configuration , inside HAL_Init() (HSI is the source clock.)
HAL_Init() is the first function called inside main();
Check , if in this infinite waiting loop the MCU is in Handler or Thread mode (if is any interrupt active and not handled by software) Check also if SysTick_Handler() exists and it is linked
if is posible post .ioc file
- Mark as New
- Bookmark
- Subscribe
- Mute
- Subscribe to RSS Feed
- Permalink
- Email to a Friend
- Report Inappropriate Content
‎2018-06-15 11:59 AM
Well whether the SysTick increments or not is a different issue (in presence of freeRTOS the HAL tick source may be defined as some other timer, not SysTick). The real issue is that
__HAL_RCC_GET_FLAG(RCC_FLAG_HSERDY) will not return SET for a long time. This means a problem with your ext. oscillator config (wrong mode, wrong frequency).
-- pa