cancel
Showing results for 
Search instead for 
Did you mean: 

Can't build STM32F746 + LWIP project

MEsco
Associate II

I created a project for using the STM32F746 DISCOVERY board with LwIP utility (see image 1 and 2 ). As soon as the project was created i tried to build it but ended up not beeing able to do so and getting the following error(see image 3):

Hope someone can help to deal with this. 

Thanks.

This discussion is locked. Please start a new topic to ask your question.
2 REPLIES 2
Piranha
Chief II

The first error says very clearly what is the problem. Maybe try actually reading it...

Hi piranha,

My problem is that the file is in the correct folder but i do not understand why this error is appearing. Also why there is a problem with a third party library given by Stm