2017-04-24 8:17 AM
Hi
i am working with CAN of STM32F303K8 when i use
status = HAL_CAN_Receive(&hcan, CAN_FIFO1, 100);
status always HAL_TIMEOUT
any help please
#can #stm32-can #nucleo-f303 #stm322017-04-24 9:26 AM
Perhaps it is not receiving anything? Is 100ms long enough? Do you have some filter settings that would exclude all traffic? Do you have the wrong data rate set up?
2017-04-24 12:52 PM
i did use an
filter
and this my config
static CanTxMsgTypeDef TxMessage;
static CanRxMsgTypeDef RxMessage;
hcan.Instance = CAN;
hcan.pTxMsg = &TxMessage;
hcan.pRxMsg = &RxMessage;
hcan.Instance = CAN;
hcan.Init.Prescaler = 2;
hcan.Init.Mode = CAN_MODE_NORMAL;
hcan.Init.SJW = CAN_SJW_1TQ;
hcan.Init.BS1 = CAN_BS1_11TQ;
hcan.Init.BS2 = CAN_BS2_4TQ;
hcan.Init.TTCM = DISABLE;
hcan.Init.ABOM = DISABLE;
hcan.Init.AWUM = DISABLE;
hcan.Init.NART = DISABLE;
hcan.Init.RFLM = DISABLE;
hcan.Init.TXFP = DISABLE;
if (HAL_CAN_Init(&hcan) != HAL_OK)
{
Error_Handler();
}
2017-04-24 2:10 PM
i did use an filter and this my config
static CanTxMsgTypeDef TxMessage;
static CanRxMsgTypeDef RxMessage;
hcan.Instance = CAN;
hcan.pTxMsg = &TxMessage;
hcan.pRxMsg = &RxMessage;
hcan.Instance = CAN;
hcan.Init.Prescaler = 2;
hcan.Init.Mode = CAN_MODE_NORMAL;
hcan.Init.SJW = CAN_SJW_1TQ;
hcan.Init.BS1 = CAN_BS1_11TQ;
hcan.Init.BS2 = CAN_BS2_4TQ;
hcan.Init.TTCM = DISABLE;
hcan.Init.ABOM = DISABLE;
hcan.Init.AWUM = DISABLE;
hcan.Init.NART = DISABLE;
hcan.Init.RFLM = DISABLE;
hcan.Init.TXFP = DISABLE;
if (HAL_CAN_Init(&hcan) != HAL_OK)
{
Error_Handler();
}
Off a 36 MHz clock that would be 1.125 Mbaud. I don't see a filter in the PM
2017-04-25 3:27 AM