cancel
Showing results for 
Search instead for 
Did you mean: 

can STM32F103 pins supply this much current in total?

mehmet.karakaya
Associate III
Posted on February 10, 2017 at 09:43

hello dear forum,

I want drive 7 segment common cathode LED display with STM32F103

if I turn on all the segments 10 x 8 = 80 mA total

can the STM32F103 supply this much current in total?

thank you

This discussion is locked. Please start a new topic to ask your question.
2 REPLIES 2
T J
Lead
Posted on February 10, 2017 at 10:18

Yes, I think all pins can generally deliver 20mA, but the total is maximum about 100mA

so you are stressing the part...

you should use a buffer, like...

http://www.digikey.com/product-detail/en/nexperia-usa-inc/74HC9115D,112/568-2752-5-ND/1023027

then the processor will be fine...

I checked the data sheet, yes 25mA max per pin and 150mA max for the whole package...

but your not being nice...

it will get warm and the Vref will not be greatly accurate.. due to the excessive heat

are you reading any A/Ds ?

________________

Attachments :

STM32F103.pdf : https://st--c.eu10.content.force.com/sfc/dist/version/download/?oid=00Db0000000YtG6&ids=0680X000006HyxI&d=%2Fa%2F0X0000000bEM%2F_7BjUE.9kdqJfuRRDBocgWPxU_V9kfiDbsI58UCj1ac&asPdf=false
David SIORPAES
ST Employee
Posted on February 10, 2017 at 10:28

Yes, you can drive up to 20mA but with relaxed Vol/Voh except PC13, PC14, PC15 which can drive only 3mA.

See page 65 of the datasheet and table 36 for actual voltage drop numbers you will incur.