cancel
Showing results for 
Search instead for 
Did you mean: 

Can one use the same .hex file to program both the STM32F446RET6 and STM32F446RCT6?

Sawd
Associate

The STM32F446RET6 and STM32F446RCT6 are similar except for Flash size. Is it possible to create a .hex file that programs the RE version that could program both chips using the ST-Link V2?

1 REPLY 1

If the image fits in the smaller flash you should be able to create a single image.

The flash size is in a variable you can recover from the System/OTP memory space.

The size frequently refers to how much of the flash memory on the die was tested, as this is a significant cost in terms of test time and throughput.

Tips, Buy me a coffee, or three.. PayPal Venmo
Up vote any posts that you find helpful, it shows what's working..