cancel
Showing results for 
Search instead for 
Did you mean: 

CAN no connection

jpeacock2399
Associate II
Posted on December 13, 2013 at 17:20

CAN requires at least two nodes in order to work.  I'm trying to determine what the error signature is for a node that is not connected to the network so that the node can go into a timed sleep/retry mode rather than constantly report errors in the CAN SCE interrupt.  For example, in a multiple node network one node starts before all others, but since no other nodes are present it looks like the node is not connected.  But I haven't been able to identify the sequence of errors (TEC, REC, EPV, EWG, BOf flags) that are unique to a disconnected node.

Has anyone worked out how to discriminate between normal CAN bus errors and a physical disconnection?

  Jack Peacock

#can
This discussion is locked. Please start a new topic to ask your question.
0 REPLIES 0