cancel
Showing results for 
Search instead for 
Did you mean: 

Can I use the WWDG to generate an interrupt when the watchdog down-counter register reaches 0x40 (EWI in WWDG_CFR is set), but keep WDGA bit cleared so that a reset is not generated ? From the block diagram, this seems like it would work.

gahelton1
Associate III
 
This discussion is locked. Please start a new topic to ask your question.
1 REPLY 1
TDK
Super User

Yes, you can reload the WWDG in the EWI interrupt to avoid a reset.

If you feel a post has answered your question, please click "Accept as Solution".