2013-05-06 06:53 AM
is it possible to interface stm32f3 discovery kit to Computer through CAN protocol ??
if yes please send me the block diagram and driver IC which is to be used .2013-05-06 08:14 AM
Review the schematic for the STM32303C-EVAL board.
http://www.st.com/web/catalog/tools/FM116/SC959/SS1532/PF252996
Apply that knowledge to the STM32F3-Discovery2013-05-06 12:04 PM
can i interface stm32f3 discovery kit to Computer through CAN protocol ??
sure you can if your computer can CAN ( I know of no PC that can CAN ) Erik2013-05-06 01:30 PM
Forgive - could not resist:
Along w/PC which ''can CAN'' - system must be ''tolerance tolerant'' as well... Likely that USB to CAN or RS232 to CAN accessory boards are in this fellow's search path...2013-05-07 05:54 AM
2013-05-07 08:48 AM
i also need code to implement but in demo folder no demo is given , from where i can get the code for CAN protocol . ?
STM32F30x_DSP_StdPeriph_Lib_V1.0.0\Project\STM32F30x_StdPeriph_Examples\CAN\CAN_LoopBackhttp://www.st.com/web/en/catalog/tools/PF258144