2013-12-17 1:25 PM
We need (don't ask why) to use a PHY which does not have COL, CRS or RX_ER pins. Can these be tied off to appropriate logic levels on the STM32F407xx we're going to be using and still result in proper operation?
Thanks,Scott #stm32 #stm32f407-mii #rx_er2013-12-17 1:54 PM
Pretty shallow pool here, suggest you contact an FAE.
Plan B would be to modify an existing board, or just not configure/connect the pins (AF mux), and try it.2013-12-17 1:58 PM
Thanks, I'll do that!
Scott2014-05-13 1:55 AM
Scott, did you ever get an answer from STM? I'm connecting the STM to RMII switch (no need for RX_ER signal because of store-and-forward). I'm want the RX_ER pins for a another function, but can't really tell from the STM32 datasheet what will happen if an input is not assigned to an alternate function.
2014-10-07 5:06 AM
Hi Scott,
I have the same question. Did you get an answer or have a solution for the ''MII-Lite'' connection?? regards Marc