2019-11-08 4:50 AM
Hello, I want to read all message coming from sensor using CAN bus. My configuration seems not okay because the CAN RX interrupt is not trigger. I made the code with CubeMX and below are my files:
Main.c
#include "main.h"
/* Private includes ----------------------------------------------------------*/
/* USER CODE BEGIN Includes */
/* USER CODE END Includes */
/* Private typedef -----------------------------------------------------------*/
/* USER CODE BEGIN PTD */
/* USER CODE END PTD */
/* Private define ------------------------------------------------------------*/
/* USER CODE BEGIN PD */
#define UART_TX_BUFFER 8
#define CAN_RX_BUFFER 8
//#define CAN1 1
/* USER CODE END PD */
/* Private macro -------------------------------------------------------------*/
/* USER CODE BEGIN PM */
/* USER CODE END PM */
/* Private variables ---------------------------------------------------------*/
CAN_HandleTypeDef hcan;
TIM_HandleTypeDef htim1;
TIM_HandleTypeDef htim2;
TIM_HandleTypeDef htim3;
TIM_HandleTypeDef htim4;
UART_HandleTypeDef huart1;
UART_HandleTypeDef huart2;
UART_HandleTypeDef huart3;
DMA_HandleTypeDef hdma_usart1_rx;
DMA_HandleTypeDef hdma_usart1_tx;
DMA_HandleTypeDef hdma_usart2_rx;
DMA_HandleTypeDef hdma_usart2_tx;
DMA_HandleTypeDef hdma_usart3_rx;
DMA_HandleTypeDef hdma_usart3_tx;
/* USER CODE BEGIN PV */
uint8_t canCheckTX = 0;
uint8_t canCheckRX = 0;
/* USER CODE END PV */
/* Private function prototypes -----------------------------------------------*/
void SystemClock_Config(void);
static void MX_GPIO_Init(void);
static void MX_DMA_Init(void);
static void MX_CAN_Init(void);
static void MX_TIM1_Init(void);
static void MX_TIM2_Init(void);
static void MX_TIM3_Init(void);
static void MX_TIM4_Init(void);
static void MX_USART1_UART_Init(void);
static void MX_USART2_UART_Init(void);
static void MX_USART3_UART_Init(void);
/* USER CODE BEGIN PFP */
/* USER CODE END PFP */
/* Private user code ---------------------------------------------------------*/
/* USER CODE BEGIN 0 */
uint8_t uart1Data[UART_TX_BUFFER];
CAN_RxHeaderTypeDef pHeader;
CAN_TxHeaderTypeDef ptHeader;
uint8_t canRxData[CAN_RX_BUFFER];
uint8_t canRxData1 = 29;
CAN_FilterTypeDef sFilterConfig;
uint8_t canTxData =10;
uint32_t TxMailBox;
/* USER CODE END 0 */
/**
* @brief The application entry point.
* @retval int
*/
int main(void)
{
/* USER CODE BEGIN 1 */
/* USER CODE END 1 */
/* MCU Configuration--------------------------------------------------------*/
/* Reset of all peripherals, Initializes the Flash interface and the Systick. */
HAL_Init();
/* USER CODE BEGIN Init */
/* USER CODE END Init */
/* Configure the system clock */
SystemClock_Config();
/* USER CODE BEGIN SysInit */
/* USER CODE END SysInit */
/* Initialize all configured peripherals */
MX_GPIO_Init();
MX_DMA_Init();
MX_CAN_Init();
MX_TIM1_Init();
MX_TIM2_Init();
MX_TIM3_Init();
MX_TIM4_Init();
MX_USART1_UART_Init();
MX_USART2_UART_Init();
MX_USART3_UART_Init();
/* USER CODE BEGIN 2 */
HAL_CAN_MspInit(&hcan);
uint8_t i = 0;
uint8_t dt = 56;
for (i = 0; i< UART_TX_BUFFER; i++)
{
uart1Data[i] = 48 + i;
}
//canRx.StdId = 0x00; //the standard identifier.
ptHeader.DLC = 8; //length of the frame that will be transmitted.
ptHeader.IDE = CAN_ID_STD; //identifier for the message that will be transmitted.
ptHeader.RTR = CAN_RTR_DATA;//the type of frame for the message that will be transmitted.
ptHeader.StdId = 0x244;
sFilterConfig.FilterFIFOAssignment = CAN_FILTER_FIFO0;
sFilterConfig.FilterIdHigh = 0x0000;
sFilterConfig.FilterIdLow = 0x0000;
sFilterConfig.FilterMaskIdHigh = 0x0000;
sFilterConfig.FilterMaskIdLow = 0x0000;
sFilterConfig.FilterBank = 0;
sFilterConfig.FilterScale = CAN_FILTERSCALE_32BIT;
sFilterConfig.FilterMode = CAN_FILTERMODE_IDMASK;
sFilterConfig.FilterFIFOAssignment = CAN_RX_FIFO0;
sFilterConfig.FilterActivation = ENABLE;
sFilterConfig.SlaveStartFilterBank = 14;
HAL_CAN_ConfigFilter(&hcan,&sFilterConfig);
HAL_CAN_Start(&hcan);
HAL_CAN_ActivateNotification(&hcan,CAN_IT_RX_FIFO0_MSG_PENDING);
//canRx.Timestamp = 1;
//canRx.FilterMatchIndex = 0x00;
/* USER CODE END 2 */
/* Infinite loop */
/* USER CODE BEGIN WHILE */
while (1)
{
/* USER CODE END WHILE */
/* USER CODE BEGIN 3 */
//HAL_StatusTypeDef HAL_CAN_GetRxMessage(CAN_HandleTypeDef *hcan, uint32_t RxFifo, CAN_RxHeaderTypeDef *pHeader, uint8_t aData[]);
//HAL_CAN_GetRxMessage(&hcan, CAN_RX_FIFO0, &canRx,canRxData);
//HAL_Delay(10);
HAL_Delay(10);
//HAL_CAN_AddTxMessage(&hcan, &ptHeader, uart1Data, &TxMailBox);
if (canCheckRX == 1)
HAL_UART_Transmit(&huart1, &canRxData1, 1, 0);
//HAL_UART_Transmit(&huart1, &canRxData1, pHeader.DLC, 1);
}
/* USER CODE END 3 */
}stm32f1xx_it.c
#include "main.h"
#include "stm32f1xx_it.h"
/* Private includes ----------------------------------------------------------*/
/* USER CODE BEGIN Includes */
/* USER CODE END Includes */
/* Private typedef -----------------------------------------------------------*/
/* USER CODE BEGIN TD */
/* USER CODE END TD */
/* Private define ------------------------------------------------------------*/
/* USER CODE BEGIN PD */
/* USER CODE END PD */
/* Private macro -------------------------------------------------------------*/
/* USER CODE BEGIN PM */
/* USER CODE END PM */
/* Private variables ---------------------------------------------------------*/
/* USER CODE BEGIN PV */
/* USER CODE END PV */
/* Private function prototypes -----------------------------------------------*/
/* USER CODE BEGIN PFP */
/* USER CODE END PFP */
/* Private user code ---------------------------------------------------------*/
/* USER CODE BEGIN 0 */
/* USER CODE END 0 */
/* External variables --------------------------------------------------------*/
extern CAN_HandleTypeDef hcan;
extern DMA_HandleTypeDef hdma_usart1_rx;
extern DMA_HandleTypeDef hdma_usart1_tx;
extern DMA_HandleTypeDef hdma_usart2_rx;
extern DMA_HandleTypeDef hdma_usart2_tx;
extern DMA_HandleTypeDef hdma_usart3_rx;
extern DMA_HandleTypeDef hdma_usart3_tx;
/* USER CODE BEGIN EV */
extern UART_HandleTypeDef huart1;
extern uint8_t uart1Data[];
extern CAN_RxHeaderTypeDef pHeader;
extern CAN_TxHeaderTypeDef ptHeader;
extern uint8_t canRxData[];
extern uint8_t canRxData1;
extern CAN_FilterTypeDef sFilterConfig;
extern uint8_t canTxData;
extern uint32_t TxMailBox;
extern uint8_t canCheckTX;
extern uint8_t canCheckRX;
void USB_LP_CAN1_RX0_IRQHandler(void)
{
/* USER CODE BEGIN USB_LP_CAN1_RX0_IRQn 0 */
/* USER CODE END USB_LP_CAN1_RX0_IRQn 0 */
HAL_CAN_IRQHandler(&hcan);
/* USER CODE BEGIN USB_LP_CAN1_RX0_IRQn 1 */
//HAL_CAN_GetRxMessage(&hcan, CAN_RX_FIFO0, &pHeader, canRxData);
//HAL_UART_Transmit(&huart1, &canRxData1, 1, 1);
canCheckRX = 1;
/* USER CODE END USB_LP_CAN1_RX0_IRQn 1 */
}Could I have your advice?
Thanks in advance!