2011-01-05 1:35 PM
Calculation error with long
2011-05-17 5:20 AM
The L suffix means long (32-bit), not long long (64-bit)
This works in Keil, other combinations result in ''integer operation result is out of range'' long long a = (long long)-1154800 * (long long)3289; Probably handled by the preprocessor, at the very least it should be folded by the optimizer. The LL suffix also works. long a = -1154800 * 3289; long long b = -1154800 * 3289; long long c = -1154800L * 3289L; long long d = (long long)-1154800 * (long long)3289; long long e = -1154800LL * 3289LL; printf(''a %ld\n'',a); printf(''b %lf\n'',(double)b); printf(''c %lf\n'',(double)c); printf(''d %lf\n'',(double)d); printf(''e %lf\n'',(double)e); a 496830096 b 496830096.000000 c 496830096.000000 d -3798137200.000000 e -3798137200.0000002011-05-17 5:20 AM
Hi Clive.
I've tried the ''long long'' method, but it didn't work.
long long e = -1154800LL * 3289LL;
This still resulted in the 496... number!
Thomas
2011-05-17 5:20 AM
Appears to function as expected with GNU 4.3.0, both d) and e) create the correct value.
Using built-in specs. Target: arm-eabi Configured with: ../gcc-4.3.0/configure --with-pkgversion='WinARM March 2008' --with-bugurl=http://en.mikrocontroller.net/forum/17 --target=arm-eabi --prefix=/c/WinARM --disable-nls --disable-shared --disable-threads --with-gcc --with-gnu-ld --with-gnu-as --enable-languages=c,c++ --enable-interwork --enable-multilib --disable-libssp --disable-libstdcxx-pch --disable-libmudflap --disable-win32-registry --disable-libgomp --with-dwarf2 --program-prefix=arm-eabi- --with-newlib --disable-newlib-supplied-syscalls --disable-libunwind-exceptions --disable-newlib-atexit-dynamic-alloc --with-gmp=/c/winarms/build/gmp_mpfr --with-mpfr=/c/winarms/build/gmp_mpfr -v Thread model: single gcc version 4.3.0 (WinARM March 2008) void write32(long addr, long x) { *((long *)addr) = x; } void write64(long addr, long long x) { *((long long *)addr) = x; } { long a = -1154800 * 3289; long long b = -1154800 * 3289; long long c = -1154800L * 3289L; long long d = (long long)-1154800 * (long long)3289; long long e = -1154800LL * 3289LL; write32(0x20002000,a); write64(0x20002010,b); write64(0x20002020,c); write64(0x20002030,d); write64(0x20002040,e); } 000001E8 A013 add r0, pc, #76 ; (adr r0, $000238=$1D9D0690) 000001EA C803 ldmia r0!, {r0, r1} ; Load incorrect 64-bit 000001EC 4B18 ldr r3, [pc, #96] ; ($000250=$20002000) 000001EE 4A19 ldr r2, [pc, #100] ; ($000254=$1D9D0690) Load incorrect 32-bit 000001F0 601A str r2, [r3, #0] 000001F2 3310 adds r3, #16 000001F4 E883 0003 stmia.w r3, {r0, r1} 000001F8 3310 adds r3, #16 000001FA E883 0003 stmia.w r3, {r0, r1} 000001FE A010 add r0, pc, #64 ; (adr r0, $000240=$1D9D0690) 00000200 C803 ldmia r0!, {r0, r1} ; Load correct 64-bit 00000202 3310 adds r3, #16 00000204 E883 0003 stmia.w r3, {r0, r1} 00000208 3310 adds r3, #16 0000020A E883 0003 stmia.w r3, {r0, r1} 00000238 1D9D0690 dd $1D9D0690 ; 64-bit WRONG 0000023C 00000000 dd $00000000 00000240 1D9D0690 dd $1D9D0690 ; 64-bit CORRECT 00000244 FFFFFFFF dd $FFFFFFFF 00000248 2000000A dd $2000000A 0000024C 40011000 dd $40011000 00000250 20002000 dd $20002000 00000254 1D9D0690 dd $1D9D0690 ; 32-bit WRONG 00000258 000AFFFF dd $000AFFFF2011-05-17 5:20 AM
Hi.
Now the calculation is correct too, when I just type in numbers. Though Ride7 and the RLINK debugger still shows the decimal representation wrong, as it can't show 64-bit numbers. But if I look in the RAM, the 8MSB's are F's - so the number is: 0xFFFFFFFF1D9D0690, which is correct.
Though if I just change my calibration matrix variables to long long, the code doesn't work at all, as the calculated x and y is over the screen limit - which shouldn't occour, but it occours on calculation errors.
The calibration matrix code and more can be seen here:
The analog readings go from 0 to 4096. The calibration code works fine on another screen with 320x240 resolution, but on the 800x480 resolution it doesn't work!
Best Regards
Thomas Jespersen
2011-05-17 5:20 AM
Do you have some real world examples for touchptr readings? And some test analogue readings.
2011-05-17 5:20 AM
Ok, your POINT structure should use signed integers (int) as some of your computation generate negative numbers as POINT values are subtracted from each other, and unless casted will be handled as (unsigned int). This was specifically important with the computation of divisor when I tried casting to (double).
The coefficients seem to be correctly computed. In the computation of x and y, you need to use 64-bit temporary results, x and y can remain as 32-bit signed long. x = (((long long)matrix.An * xAnalogReading) + ((long long)matrix.Bn * yAnalogReading) + matrix.Cn) / matrix.Divider; y = (((long long)matrix.Dn * xAnalogReading) + ((long long)matrix.En * yAnalogReading) + matrix.Fn) / matrix.Divider;